Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

【ION9000 PM8000 】V4.7.1 Template Data

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • 【ION9000 PM8000 】V4.7.1 Template Data
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Miyai
Miyai
Contributor

Posted: ‎2026-03-26 10:08 PM

0 Likes
2
631
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
‎2026-03-26 10:08 PM

【ION9000 PM8000 】V4.7.1 Template Data

Hello,


Where can I download V4.7.1 template for ION9000 and PM8000?


I checked V4.7.1 firmware folder,

However, template included was version 4.6.0..

 

I would like to check out the 6-output option module, which was added in V4.7.1.

 

 

Regards,

Miyai

 

Labels
  • Labels:
  • ION9000
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-03-30 09:32 AM

0 Likes
1
626
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
‎2026-03-30 09:32 AM

Hello @Miyai 

V4.7.1 did not make any changes to the default template therefore the template version was not changed. Note that the 6 Digital output module is not yet commercialized so there is currently nothing that can be checked out. The firmware work was completed in V4.7.1 so that when hardware is released the meter's support the module. 

 

The firmware change as far as modules goes is meter can now support an additional 4 Digital output modules.

 

The default template has 2 digital output modules created for each possible IO module slot. The 6 DO module will also use that same 2 Digital output module. If ION Setup detects that a 6 DO module is present on the meter, ION Setup will make 4 new Digital Output modules. In Designer a user will need to make 4 additional Digital output modules and assign to the 6DO module.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-03-30 09:32 AM

0 Likes
1
626
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
‎2026-03-30 09:32 AM

Hello @Miyai 

V4.7.1 did not make any changes to the default template therefore the template version was not changed. Note that the 6 Digital output module is not yet commercialized so there is currently nothing that can be checked out. The firmware work was completed in V4.7.1 so that when hardware is released the meter's support the module. 

 

The firmware change as far as modules goes is meter can now support an additional 4 Digital output modules.

 

The default template has 2 digital output modules created for each possible IO module slot. The 6 DO module will also use that same 2 Digital output module. If ION Setup detects that a 6 DO module is present on the meter, ION Setup will make 4 new Digital Output modules. In Designer a user will need to make 4 additional Digital output modules and assign to the 6DO module.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Miyai
Miyai
Contributor

Posted: ‎2026-03-31 08:10 PM

0 Likes
0
611
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
‎2026-03-31 08:10 PM

Hello, @Charles_Murison 

 

Thank you for your support.

I will wait for release of 6 digital output module.

 

 

Regards,

Miyai
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.