Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION9000 Logging two sources

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION9000 Logging two sources
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Anonymous user
Not applicable

Posted: ‎2020-03-05 02:59 AM

0 Likes
4
2097
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
‎2020-03-05 02:59 AM

ION9000 Logging two sources

Is there an effective way of logging energy usage and power on an ION9000 from two different sources ?

 

Situation is that we have a site with a generator and mains incoming supply both upstream of the ION9000 with one set of CT's and Vrefs, can we give a digital input to the meter and have it log energy or other measurement to a different register so we can report in PME on just generator usage ?

 

Layout like this:

 

Mains    Gen

    |            |

   X           X         ION

    |            |            |

    ---------------------0------->

       

Anybody done anything like this and care to share the process ?

Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-03-06 10:41 AM

1 Like
0
2073
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
‎2020-03-06 10:41 AM

Hello Grant,

 

Many of the alarms come from set point modules, these modules have an Enable input. You could link the enable input to the Digital input state. 

 

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 4
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-03-05 09:08 AM

0 Likes
0
2092
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
‎2020-03-05 09:08 AM

Hello Rich,

 

The digital input can be linked to the enable of the integrator module, you would be able to turn energy accumulation on and off using the digital input. This could be applied to integrators for the main and generator. Sliding Window demand can also be setup like this as well as data recorders. Depending on what measurements you want you can likely do this.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
DanL
DanL Champion
Champion

Posted: ‎2020-03-05 01:32 PM

1 Like
2
2081
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
‎2020-03-05 01:32 PM

Have a look at the Conditional Energy feature in the default template
https://www.productinfo.schneider-electric.com/ion9000/viewer?docidentity=ConditionalEnergy-5546D2B4...

 

Reply
Grant_IPACS
Grant_IPACS
Mentor

Posted: ‎2020-03-05 09:29 PM

0 Likes
1
2077
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
‎2020-03-05 09:29 PM

Wondering if i can apply this to a circuit for monitoring generator circuit only... as it is normally zero... maybe halt logging while gen not running, as meter currently logs many errors when generator is off... can we suppress alarms such as low volt, when say DI1 (Gen run) input is off?

Regards

Grant
Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2020-03-06 10:41 AM

1 Like
0
2073
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
‎2020-03-06 10:41 AM

Hello Grant,

 

Many of the alarms come from set point modules, these modules have an Enable input. You could link the enable input to the Digital input state. 

 

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.