Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION9000 IEC61850

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION9000 IEC61850
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Wojtek_1980
Wojtek_1980
Explorer

Posted: ‎2026-03-02 11:28 PM

0 Likes
3
701
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
‎2026-03-02 11:28 PM

ION9000 IEC61850

The ION9000 meter operates in the IEC61850 protocol, and that's clear. And now we have an optical IEC61850 loop (HSR) composed of SIEMENS protection relays from the SIPROTEC 5 family. We need to add our four ION9000s to this loop. How do we solve this? My thinking is this: If the ION9000s support the HSR architecture, they can be connected to the existing loop along with the SIPROTECs! We then need to use opto/twisted-pair converters in the IEC61850 loop. Is this connection acceptable? Has anyone else experienced this problem? If not, we will need to use a REDBOX (HSR/PRP converter), which will connect the ION9000s and allow them to be connected to the existing IEC61850 loop with the SIPRPTEC.

Labels
  • Labels:
  • ION9000
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-03-09 09:13 AM

0 Likes
0
580
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
‎2026-03-09 09:13 AM

Hello @Wojtek_1980 ,

 

The ION9000 meters support IEC61850 MMS. The meter could be connected to RedBox (Redundancy Box) such that single-attached traffic (SAN) is directed to the meter. This can still use IEC61850, and does not have to use Modbus.

 

I myself do not have any experience with such a setup.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 3
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-03-03 02:09 AM

0 Likes
2
696
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
‎2026-03-03 02:09 AM

Hello @Wojtek_1980,


The ION9000 does not support HSR/PRP. The meter does support Rapid Spanning Tree Protocol, RSTP however I believe PRP is different protocol.

 

As for options, I cannot give any suggestions but hopefully someone else can give their experience.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
Wojtek_1980
Wojtek_1980
Explorer

Posted: ‎2026-03-04 04:12 AM

0 Likes
1
630
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
‎2026-03-04 04:12 AM

Thank You @Charles_Murison 

 

So , it is not possible to use the ION9000 in the final version of IEC61850 (HSR) or in an IEC61850 radial network (PRP)? Did someone has an expirience of such connections ???

How do I connect four ION9000 meters (i.e., MODBUS TCP/IP) to the IEC61850 optical level? Does anyone have any ideas? Perhaps as follows?

1) Connect four ION9000 meters using an Ethernet device.
2) Convert MODBUS TCP/IP to IEC61850 using a network gateway.
3) Connect to the IEC61850 fiber optic port using a REDBOX device (HSR/PRP converter).

 

OR MAYBE
In the ION 9000 TECHNICAL MANUAL, in the "Protocols, Ports, and Connections" section, we can read that the ION9000 supports the IEC61850 standard.

So, after adding a REDBOX (HSR to PRP converter), I should connect the ION group to the existing SIPROTEC 5 fiber optic ring from SIEMENS.

Does anyone have experience with such connections?

 

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-03-09 09:13 AM

0 Likes
0
581
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
‎2026-03-09 09:13 AM

Hello @Wojtek_1980 ,

 

The ION9000 meters support IEC61850 MMS. The meter could be connected to RedBox (Redundancy Box) such that single-attached traffic (SAN) is directed to the meter. This can still use IEC61850, and does not have to use Modbus.

 

I myself do not have any experience with such a setup.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.