Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84294members
353433posts

ION8650 Firmware - Hashes and Files

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Sanjeet_Sahota
Lieutenant Lieutenant
Lieutenant

ION8650 Firmware - Hashes and Files

Hello All

 

In an effort to provide more ways to validate that the file you are using to upgrade your meter I have created this table of hashes of the firmware for our released file.  

 

Firmware Version

SHA256 Hash

V004.020.001A

95F4AB3C8F5EEE6AEE618FDA31FF617375C4A8CB427A5A4ED038CD8E3A26FF84

V004.020.001B

D91D352A2A2E6222A5C77A667EAEC156B878174B90E0B3751B8BC7042F89B515

V004.020.001C

4FBC04A5B9897C63F00356A2B674AB3E34C59254CC8264465401B5EAB4B51D50

 

 

V004.021.000A

E0D5F3F496723D22E343FB8BEAFC98680A9B3506DC7FD9BB82B2D947892EC06E

V004.021.000B

651F90D3264D228763A06C38837832B5EAD5E67C9C69E2969D821F4AF00D3C11

V004.021.000C

A356B48AF1468D1D3605BC40BE2989C56101A0FE2AE5DE5B5D9A126EA030E2B7

 

 

V004.031.002A

BED35EE1760FE3A159A58377E917AA51ECAF4A3846B89280AFD95A18EDA951C0

V004.031.002B

48C3B439357A5B903EBD083094E38FC62611D09F3744B0FE930FC0B19EC3D979

V004.031.002C

C95567CDDE4861DCB1E45478736372408A4ED005B9CA72FA506F68F1EF11759D

 

 

V004.040.001A

A2CB7456167846A879D9017A854A9E94E1958B970ECEC45C9F4B7515A8682908

V004.040.001B

E70620A8E2CC12FB8702D31105C0DDD12321AD62360DBA22B088C212F23C73EC

V004.040.001C

1A6E5D5233EBCF7653BEA8ACEB2019A2F219860B58C4541E29F21E082E468B29

 


Two options for performing checksum calculations on downloaded files are shown below. Only one needs to be used. Choose the option that is most convenient for you. Compare your results to the values provided in the table below. The results are not case sensitive (upper case letters are considered the same as its corresponding lower case letter).

 

7-Zip Method


7-Zip is a free and open source program for managing compressed files such as .zip, .tar.gz, and .rar files.  File checksums can be performed with the Windows Explorer Right Click Menu provided by the latest 7-Zip Version, if you have it enabled in the 7-Zip options, as shown below:

Image1.jpg

 

Once completed, right click on the extracted firmware file in Windows explorer and choose CRC SHA -> SHA256

 

Missing image.jpg

 

Validate that the checksum matches the listed hash above for the corresponding firmware version.

 


Notepad++ Method

 

Alternatively, Notepad++, a free and open-source alternative, can be used to generate SHA-256 hashes for files.  To calculate the hash on a file, click the Tools-> SHA-256 -Generate from files... menu option

 

Image 2.jpg

 

Next, click on the Choose Files to generate SHA-256... button and navigate to the firmware file to be verified

 

Image 3.jpg

 

The hash can be found in the box below.  Compare this value to the value found in the post above.

 

Image 4.jpg

 

 

Thanks to Chris Kerr for providing the steps above.  I will continue to update this post with more firmware versions.

 

 

Attachments

Accepted Solutions
Charles_Murison
Picard Picard
Picard
0
3264

Re: ION8650 Firmware - V4.20 and Later - Hashes and Files

Thank you Sanjeet for providing this information

L4 Prime for Advanced metering and Utilities

See Answer In Context

Tags (1)
1 Reply 1
Charles_Murison
Picard Picard
Picard
0
3265

Re: ION8650 Firmware - V4.20 and Later - Hashes and Files

Thank you Sanjeet for providing this information

L4 Prime for Advanced metering and Utilities
Tags (1)