Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION8600 V332 - Data Recorder / Revenue Log retrieval via Modbus (43001 - 43153)

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION8600 V332 - Data Recorder / Revenue Log retrieval via Modbus (43001 - 43153)
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
582
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
digowstm
digowstm
Explorer

Posted: ‎2026-09-16 11:36 AM

0 Likes
1
167
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
‎2026-09-16 11:36 AM

ION8600 V332 - Data Recorder / Revenue Log retrieval via Modbus (43001 - 43153)

Hello,

We are evaluating the retrieval of historical Load Profile / Revenue Log data from a PowerLogic ION8600 running firmware 8600V332 using Modbus.

We are referring to document 70022-0124-01, specifically Appendix B - Data Record / Modbus Map, which describes Data Recorder retrieval using registers 43001-43153.

We found Schneider FAQ FAQ000268832, which demonstrates this procedure on an ION8650. We also found the community discussions “Reading Revenue Log Data on ION 8650 via Modbus” and “Extract Data Recorder registers in PM8000/ION9000 with modbus protocol.”

From those references, we understand that Data Recorder retrieval through Modbus is supported on the ION8650, while PM8000/ION9000 do not support this mechanism.

We would therefore like to confirm specifically for the ION8600:

1. Does the Data Record / Modbus Map described in Appendix B (registers 43001-43153) support an ION8600 running firmware 8600V332?

2. The meter is configured with "Allow Modbus Programing = No". Does this setting prevent the control writes required by the retrieval procedure, specifically:

  • writing the Data Recorder Module Number to 43001;
  • writing the Starting Record to 43002-43003?

Our intention is only to retrieve existing historical records. We do not intend to modify the Data Recorder setup, framework, sources, logging interval, depth, or any other meter configuration.

From Appendix B, our understanding is that these writes are part of the Data Recorder selection/retrieval mechanism rather than changes to the Data Recorder setup. Could you please confirm whether this interpretation is correct for the ION8600?

Thank you.

Labels
  • Labels:
  • ION8000
Tags (5)
  • Tags:
  • data recorder
  • english
  • historical data
  • ion8600
  • modbus
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2026-09-17 01:19 PM

1 Like
0
155
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
‎2026-09-17 01:19 PM

Hi @digowstm

 

1. Does the Data Record / Modbus Map described in Appendix B (registers 43001-43153) support an ION8600 running firmware 8600V332?
Firmware V330 or higher supports the procedures outlined Appendix B in the Modbus Map document.

 

2. The meter is configured with "Allow Modbus Programing = No". Does this setting prevent the control writes required by the retrieval procedure, specifically:

writing the Data Recorder Module Number to 43001;
writing the Starting Record to 43002-43003?

As I tested both conditions, with "Allow Modbus Programming" enabled and disabled, I was able to successfully write to and read from the Data Recorders via Modbus.

Mehran_Mehrnia_0-1789676216298.png

 

Best Regards,

-Mehran

L3 Expert Advanced metering 

See Answer In Context

Reply
Reply 1
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2026-09-17 01:19 PM

1 Like
0
155
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
‎2026-09-17 01:19 PM

Hi @digowstm

 

1. Does the Data Record / Modbus Map described in Appendix B (registers 43001-43153) support an ION8600 running firmware 8600V332?
Firmware V330 or higher supports the procedures outlined Appendix B in the Modbus Map document.

 

2. The meter is configured with "Allow Modbus Programing = No". Does this setting prevent the control writes required by the retrieval procedure, specifically:

writing the Data Recorder Module Number to 43001;
writing the Starting Record to 43002-43003?

As I tested both conditions, with "Allow Modbus Programming" enabled and disabled, I was able to successfully write to and read from the Data Recorders via Modbus.

Mehran_Mehrnia_0-1789676216298.png

 

Best Regards,

-Mehran

L3 Expert Advanced metering 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.