Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION7500 Continually recycling

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Re: ION7500 Continually recycling
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
mcolston
mcolston
Troubleshooter

Posted: ‎2018-11-26 08:15 AM

0 Likes
1
1358
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
‎2018-11-26 08:15 AM

ION7500 Continually recycling

I have a customer that has a few of these meters installed - most of them are just RS485 connected to a BMS.

 

One or two of them will restart on a regular basis - sometimes will stop, and allow access to the menu's, but other ones just continually reboot.

 

Any idea what could be the cause of this? Could it be power supply issues?

 

Also, one that was resetting a lot was removed and a spare they had on site installed - this one didn't have the additional IO card, so that was installed, but is not setup. I did manage to power the old one up (Which then didn't reset for several hours) and pull off the configuration file with IONsetup. 

 

I assume there will be no issue downloading this configuration to the new meter - with perhaps the exception of it needing the ethernet port then setup?

Mark Colston
adi Intelligent Buildings Ltd
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Anonymous user
Not applicable

Posted: ‎2018-11-27 12:21 PM . Last Modified: ‎2018-11-27 12:22 PM

2 Likes
0
1356
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
‎2018-11-27 12:21 PM

Hi @mcolston,

 

It is really hard to identify what could be the issue from the information you have shared. It can be power supply yes, but other things as well.

I would advise you to contact technical support, they will help you collect the meter eventlog (for the device you have replaced and powered) to check for internal errors on the meter.

With this information it may be easier to tell what is happening ot the devices.

 

Besides that we might need the device returned to Victoria for failure analysis, but if the device is working fine after removed from the customer it may get tricky to replicate the issue and understand the root cause.

 

Please open a tech support case and share the case number and we will be able to investigate.

 

Thanks,

Fabricio

See Answer In Context

Reply
Reply 1
Anonymous user
Not applicable

Posted: ‎2018-11-27 12:21 PM . Last Modified: ‎2018-11-27 12:22 PM

2 Likes
0
1357
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
‎2018-11-27 12:21 PM

Hi @mcolston,

 

It is really hard to identify what could be the issue from the information you have shared. It can be power supply yes, but other things as well.

I would advise you to contact technical support, they will help you collect the meter eventlog (for the device you have replaced and powered) to check for internal errors on the meter.

With this information it may be easier to tell what is happening ot the devices.

 

Besides that we might need the device returned to Victoria for failure analysis, but if the device is working fine after removed from the customer it may get tricky to replicate the issue and understand the root cause.

 

Please open a tech support case and share the case number and we will be able to investigate.

 

Thanks,

Fabricio
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.