Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
When using ION setup to config the auto reset calendar in PM2230, when I choose the date to be reset and press ok, the reset calendar suppose to show the date I chosen, instead, it show a pile of meaningless character, and as expected, the command could not download to PM2230.
Is it a software bug? How to deal with it?
Link copied. Please paste this link to share this article on your social media post.
Hello @David_Kwan
This appears to be a defect in ION Setup. Could you please create a support ticket so that the issue can be investigated and addressed by the development team?
In the meantime, as a workaround, you can configure the Auto Reset Calendar using the available Modbus registers. Auto Reset for Energy and Maximum Demand parameters can be configured only
through communication.
Link copied. Please paste this link to share this article on your social media post.
Hello @David_Kwan ,
Please contact your local customer care center (CCC) to start a case. If this is an unexpected behaviour the development team will need information from the case.
If possible, are you able to record the packet traffic from the computer to the meter? For example using Wireshark. If possible, be sure to include the capture when you contact the CCC.
Regards,
Charles
Link copied. Please paste this link to share this article on your social media post.
Hello @David_Kwan
This appears to be a defect in ION Setup. Could you please create a support ticket so that the issue can be investigated and addressed by the development team?
In the meantime, as a workaround, you can configure the Auto Reset Calendar using the available Modbus registers. Auto Reset for Energy and Maximum Demand parameters can be configured only
through communication.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.