Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION Setup 3.2 and PM2230 auto reset calendar

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • ION Setup 3.2 and PM2230 auto reset calendar
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
David_Kwan
David_Kwan
Explorer

Posted: ‎2026-09-17 08:02 PM

0 Likes
2
272
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
‎2026-09-17 08:02 PM

ION Setup 3.2 and PM2230 auto reset calendar

When using ION setup to config the auto reset calendar in PM2230, when I choose the date to be reset and press ok, the reset calendar suppose to show the date I chosen, instead, it show a pile of meaningless character, and as expected, the command could not download to PM2230.

 

Is it a software bug? How to deal with it?

Labels
  • Labels:
  • ION Setup
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
akash_das
akash_das Troubleshooter
Troubleshooter

Posted: ‎2026-09-25 02:31 AM

0 Likes
0
222
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
‎2026-09-25 02:31 AM

Hello @David_Kwan 

This appears to be a defect in ION Setup. Could you please create a support ticket so that the issue can be investigated and addressed by the development team?

 

In the meantime, as a workaround, you can configure the Auto Reset Calendar using the available Modbus registers. Auto Reset for Energy and Maximum Demand parameters can be configured only
through communication.

akash_das_0-1790328581867.png

 

See Answer In Context

Reply
Replies 2
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-09-18 08:58 AM

0 Likes
0
264
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
‎2026-09-18 08:58 AM

Hello @David_Kwan ,

 

Please contact your local customer care center (CCC) to start a case. If this is an unexpected behaviour the development team will need information from the case.

If possible, are you able to record the packet traffic from the computer to the meter? For example using Wireshark. If possible, be sure to include the capture when you contact the CCC. 

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
akash_das
akash_das Troubleshooter
Troubleshooter

Posted: ‎2026-09-25 02:31 AM

0 Likes
0
222
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
‎2026-09-25 02:31 AM

Hello @David_Kwan 

This appears to be a defect in ION Setup. Could you please create a support ticket so that the issue can be investigated and addressed by the development team?

 

In the meantime, as a workaround, you can configure the Auto Reset Calendar using the available Modbus registers. Auto Reset for Energy and Maximum Demand parameters can be configured only
through communication.

akash_das_0-1790328581867.png
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.