Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

HDPM6000 Lost IP address and Modbus Serial Setting

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • HDPM6000 Lost IP address and Modbus Serial Setting
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
TC
TC Explorer
Explorer

Posted: ‎2025-12-23 12:17 AM

0 Likes
2
1195
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
‎2025-12-23 12:17 AM

HDPM6000 Lost IP address and Modbus Serial Setting

Hi there,

Customer changed IP address in HDPM6000, and then not able to communicate. Not able to ping.

Tried to find out the IP address and mask by accessing MODBUS address 4484 - 4487, also failed, using default baudrate 115200 and ID #1. (customer did try with other settings but not all possible combinations)

Customer has total 15 sets, only this particular one having such issue. 

 

Is there a way out of this other than replacing with brand new unit.

It seems no way to master reset to factory setting in this case.

Labels
  • Labels:
  • HDPM6000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-12-23 10:27 AM . Last Modified: ‎2026-04-02 11:35 AM

1 Like
1
1188
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
‎2025-12-23 10:27 AM

Hi @TC 

 

Correct. There is no master reset to factory settings and the role of the reset button is to re-initiates the communication(without power cycle the meter).

 

If meter is still operational, there are some possible workarounds to find out the configured IP address on the meter:

1- If possible, connect the PC directly to the meter and ensure to assign the computer a static IP with correct subnet mask correlated to the new IP address.

Just as a reminder, starting from firmware version V62.7 (V62 package), HTTPS and related functionality were added to the meter, requiring access via HTTPS (e.g., https://10.10.10.4).

 

2- Using NetConfig free tool for Network Discovery that can automatically discover devices on the network, provided that meter has fw version above 60, otherwise it is a read only and at least should discover the device connected to the laptop network. Temporarily disabling the firewall might be needed.

 

3- Using Wireshark tool can help discover the IP addresses of connected Ethernet devices on the same network as the PC running Wireshark. Wireshark can capture broadcast packets, including ARP (Address Resolution Protocol) requests and replies which will show the sender's IP and MAC address, along with the target IP and MAC address being requested.

 

4- Software Manager has the Discover option, but maybe works on the same IP subnet:

HDPM6000 Installation Guide:

 
 

Mehran_Mehrnia_2-1766511867159.png

 

5- You indicated that you attempted to connect via Modbus serial, but is meter entirely unresponsive over the serial Modbus interface?

By default serial Modbus settings of HDPM6000 is as below:

Default serial port settings:
Unit ID - 1
Parity - None
Stop Bits - 1
Baud Rate - 115200

If meter is responsive, you can connect serially to the device via a gateway or USB/Serial converter to read the 16 Modbus registers from 4480 from the serial port of this meter using any Modbus application to view the configured IP address of this meter.

HDPM6000 Protocol Guide:

Mehran_Mehrnia_3-1766512728477.png

In this example, I connected serially to the meter with related serial settings and polled the IP address related  registers:

Mehran_Mehrnia_4-1766513277732.png

 

Additionally, verify the meter’s LED status indicators for any error conditions:
LED on HDPM6000 Head Unit

 

If none of the above steps resolve the issue, the meter may need to be replaced.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Replies 2
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-12-23 10:27 AM . Last Modified: ‎2026-04-02 11:35 AM

1 Like
1
1188
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
‎2025-12-23 10:27 AM

Hi @TC 

 

Correct. There is no master reset to factory settings and the role of the reset button is to re-initiates the communication(without power cycle the meter).

 

If meter is still operational, there are some possible workarounds to find out the configured IP address on the meter:

1- If possible, connect the PC directly to the meter and ensure to assign the computer a static IP with correct subnet mask correlated to the new IP address.

Just as a reminder, starting from firmware version V62.7 (V62 package), HTTPS and related functionality were added to the meter, requiring access via HTTPS (e.g., https://10.10.10.4).

 

2- Using NetConfig free tool for Network Discovery that can automatically discover devices on the network, provided that meter has fw version above 60, otherwise it is a read only and at least should discover the device connected to the laptop network. Temporarily disabling the firewall might be needed.

 

3- Using Wireshark tool can help discover the IP addresses of connected Ethernet devices on the same network as the PC running Wireshark. Wireshark can capture broadcast packets, including ARP (Address Resolution Protocol) requests and replies which will show the sender's IP and MAC address, along with the target IP and MAC address being requested.

 

4- Software Manager has the Discover option, but maybe works on the same IP subnet:

HDPM6000 Installation Guide:

 
 

Mehran_Mehrnia_2-1766511867159.png

 

5- You indicated that you attempted to connect via Modbus serial, but is meter entirely unresponsive over the serial Modbus interface?

By default serial Modbus settings of HDPM6000 is as below:

Default serial port settings:
Unit ID - 1
Parity - None
Stop Bits - 1
Baud Rate - 115200

If meter is responsive, you can connect serially to the device via a gateway or USB/Serial converter to read the 16 Modbus registers from 4480 from the serial port of this meter using any Modbus application to view the configured IP address of this meter.

HDPM6000 Protocol Guide:

Mehran_Mehrnia_3-1766512728477.png

In this example, I connected serially to the meter with related serial settings and polled the IP address related  registers:

Mehran_Mehrnia_4-1766513277732.png

 

Additionally, verify the meter’s LED status indicators for any error conditions:
LED on HDPM6000 Head Unit

 

If none of the above steps resolve the issue, the meter may need to be replaced.

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
TC
TC Explorer
Explorer

Posted: ‎2026-01-01 10:48 PM

0 Likes
0
1144
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
‎2026-01-01 10:48 PM

Thanks @Mehran_Mehrnia . Customer claim that they have tried without success, and decided to file a warranty claim as the fastest way to resolve the issue of one unit out of many that working fine.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.