Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

EM4928E troubles with split core 50A output 0.333V

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Re: EM4928E troubles with split core 50A output 0.333V
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
571
Mehran_Mehrnia
Mehran_Mehrnia Champion
203
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
lsubillaga
lsubillaga
Explorer

Posted: ‎2024-10-31 03:51 PM

0 Likes
1
996
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
‎2024-10-31 03:51 PM

EM4928E troubles with split core 50A output 0.333V

Hello everyone,

 

I'm having troubles with an EM4928E. The client have split core 50A output 0.333V and they requested to use them in an EM4928E to measure a new area. When I connect one CT (50A) to the meter in phase A it shows a value of 60A in the real time reading (ION Setup) and the rest of the readings of the other channels for phase A showed altered. For example in the channel (phase A) where are installed 100A split core the reading goes to 120A and the channels (phase A) where are installed 200A split core the readings goes to 240A. The other two phases were normal. I tried moving the 50A CT to phase B and phase C and the behavior looks the same (but in the corresponding phase). I tried also another free channels and behavior still the same. 

After that, I tried with the same 50A CT in a BCPMSCE60 and it worked good. That meter showed the correct reading. So, I thought that maybe these 50A CT are not compatible with EM4928E. I looked for the documentation and I find out that they should be compatible, but they are not working.

Is there something I need to do in the configuration in ION Setup for the meter to work with these 50A split core CT?

 

I wait for your comments.

Regards,

Luis Subillaga

Labels
  • Labels:
  • HDPM6000
  • ION Setup
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2025-01-07 07:54 AM

0 Likes
0
907
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
‎2025-01-07 07:54 AM

Please connect with local technical support team. 

See Answer In Context

Reply
Reply 1
Ramasamy_N
Ramasamy_N Champion
Champion

Posted: ‎2025-01-07 07:54 AM

0 Likes
0
908
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
‎2025-01-07 07:54 AM

Please connect with local technical support team. 
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.