Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Differences in System Type Settings for the PM5560

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Differences in System Type Settings for the PM5560
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
573
Mehran_Mehrnia
Mehran_Mehrnia Champion
210
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Miyai
Miyai
Contributor

Posted: ‎2026-08-17 07:39 PM

0 Likes
1
217
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
‎2026-08-17 07:39 PM

Differences in System Type Settings for the PM5560

Hello,

 

Are there any differences in the measurement items or values ​​between the "3PH3W Dlt Ungnd" and "3PH3W Wye Ungnd" wiring settings on the PM5560?

 

I am checking the web screen and the Phaser screen, but I cannot see any difference.

 

Do the settings need to be separated for this?

 

 

Regards,

Miyai

 

Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
akash_das
akash_das Troubleshooter
Troubleshooter

Posted: ‎2026-08-18 12:20 AM

0 Likes
0
200
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
‎2026-08-18 12:20 AM

Hi @Miyai 

Your application appears to be well within the supported voltage range for both 3PH3W Dlt Ungnd and 3PH3W Wye Ungnd configurations. Therefore, it is expected that the meter would display the same line-to-line voltage measurements and a similar phasor screen in both cases.

 

However, the two settings are intended for different power system topologies and have different voltage ratings for direct connection:

 

3PH3W Dlt Ungnd (Ungrounded Delta):
Direct connection maximum: 600 V L-L (UL and IEC)
No line-to-neutral voltage reference exists in the system.

 

3PH3W Wye Ungnd (Ungrounded Wye):
Direct connection maximum: 347 V L-N / 600 V L-L (UL)
Direct connection maximum: 400 V L-N / 690 V L-L (IEC)
The system is modeled as an ungrounded wye network with phase-to-neutral voltage relationships.

 

Therefore, the wiring mode should be selected according to the actual electrical distribution system being monitored, even if the displayed measurements appear similar. Using the correct wiring configuration ensures that the meter applies the appropriate phasor relationships and voltage calculations for the installation.

See Answer In Context

Attachments
Reply
Reply 1
akash_das
akash_das Troubleshooter
Troubleshooter

Posted: ‎2026-08-18 12:20 AM

0 Likes
0
201
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
‎2026-08-18 12:20 AM

Hi @Miyai 

Your application appears to be well within the supported voltage range for both 3PH3W Dlt Ungnd and 3PH3W Wye Ungnd configurations. Therefore, it is expected that the meter would display the same line-to-line voltage measurements and a similar phasor screen in both cases.

 

However, the two settings are intended for different power system topologies and have different voltage ratings for direct connection:

 

3PH3W Dlt Ungnd (Ungrounded Delta):
Direct connection maximum: 600 V L-L (UL and IEC)
No line-to-neutral voltage reference exists in the system.

 

3PH3W Wye Ungnd (Ungrounded Wye):
Direct connection maximum: 347 V L-N / 600 V L-L (UL)
Direct connection maximum: 400 V L-N / 690 V L-L (IEC)
The system is modeled as an ungrounded wye network with phase-to-neutral voltage relationships.

 

Therefore, the wiring mode should be selected according to the actual electrical distribution system being monitored, even if the displayed measurements appear similar. Using the correct wiring configuration ensures that the meter applies the appropriate phasor relationships and voltage calculations for the installation.

Attachments
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.