Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84245members
353344posts

Commercialization New Open Toroids

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Madleen_Laclef
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
3
530

Commercialization New Open Toroids

2 new split core toroids called TOA80 and TOA120 are replacing the previous POA (ref 50485) and GOA (ref 50486).
 
TOA have been tested with Vigilohm and are now available to order. POA and GOA are being removed from the market.
 
The TOA range key advantages are:
  • its facility of installation, especially the way it is opened and closed, with no need of tools
  • it offers bigger diameters, respectively 80 and 120mm for TOA while POA was 46mm and GOA 110 mm
  • its weight (divided by more than 50%)
  • it is cheaper

 

 

Example of use:

We will order some to do a field test for a customer currently using Bender.

As their installation is live, and cannot be stopped, the open toroids are the good option to perform this test.

We hope to prove to this customer the good measurements made by our devices, versus what Bender offers.

In this particular example, the test will be done with an XML3xx, since the customer is very interested in Capacity measurements (that he does not have with Bender). He wants to know the capacitance to be able to evaluate the faulty current in case of first fault and the touch voltage, since he had accidents in the past.

 

Attachments
Tags (2)
3 Replies 3
sesa99179
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
504

Re: Commercialization New Open Toroids

Provide the key advantages and application example. easy to selection.

Madleen_Laclef
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
504

Re: Commercialization New Open Toroids

In the past, we already offered Open toroids (also called Split toroids) in the catalogue. Now we are changing their reference. The new Open toroids (versus the old Open toroids) have the advantages that are described above.

Regarding the selection of Open toroids versus Closed toroids:

> Open toroids can be wired on an installation without having to shut down the installation. In the case of brown field projects, that can be interesting. If the customer installation cannot be stopped, we can still install a locator,using Open toroids.

> The drawback is that Open toroids are always more expansive than Closed toroids. So we cannot offer this in all cases.

sesa99179
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
504

Re: Commercialization New Open Toroids

For toroid in hospitals, Bender have integrated type.

Ithink thisintegrated type in the hospital is more convenient,and less costly.

7103