Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Can the A9MEM1560 product be used for single-phase L-L 208V

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Can the A9MEM1560 product be used for single-phase L-L 208V
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
575
Mehran_Mehrnia
Mehran_Mehrnia Champion
214
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Metering & Power Quality
Start a Topic
Kwon
Kwon
Contributor

Posted: ‎2026-09-28 02:13 AM

0 Likes
2
88
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
‎2026-09-28 02:13 AM

Can the A9MEM1560 product be used for single-phase L-L 208V

Kwon_0-1790586642679.png

 

I have an additional question.

In the 208V 3-phase, 3-wire system mentioned above, if UL certification is not required,
can the A9MEM1560 be used for Power Tag Unit 1 and the A9MEM1580 for Power Tag Unit 2?

I would appreciate your help. Thank you.

Labels
  • Labels:
  • PowerTag Energy
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
AnandK
AnandK Contributor
Contributor

Posted: ‎2026-09-28 04:47 AM

2 Likes
0
78
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
‎2026-09-28 04:47 AM

Hi Kwon
As per my understanding and findings : 

A9MEM1560 is intended for single-phase (1PH2W) applications. In the proposed 208V 3P3W system, the load is connected line-to-line (L1-L2 = 208 V) and no neutral is available. 
AnandK_0-1790595845689.png
A9MEM1580: Supported for 208 V 3PH3W systems (173-480 V L-L range)
AnandK_1-1790596013871.png

 

 



Reply
Kwon
Kwon
Contributor

Posted: ‎2026-09-28 09:43 PM

0 Likes
0
52
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
‎2026-09-28 09:43 PM

Thank you for the quick reply.

In that case, this means that the only PowerTag product compatible with the "PowerTag Unit 1" (208V single-phase L-L) shown in the photo above is Product PLTQO302P, which is designed for QO-type circuit breakers.

 

However, since Fuji Electric circuit breakers are currently being used on-site, it is difficult to propose PowerTag.
Is there any way to propose a different product from the PowerTag lineup?

Thank you.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.