Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84584members
353853posts

Accusine PCSn - Minimum Current Transformer Primary Current?

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

sesa108084_brid
Lieutenant JG Lieutenant JG
Lieutenant JG

Accusine PCSn - Minimum Current Transformer Primary Current?

Good day

 

Is the minimum primary current rating for the CT has to be 100A?

My installation incomer is only 32A.


TQ
 

Attachments
1 Reply 1
LazCM_175878
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Accusine PCSn - Minimum Current Transformer Primary Current?

Hi,

yes CT sensors  must be selected according to SE recommendation:
• 5 A or 1 A secondary
• 100A to 10,000A primary rating
• 50/60 Hz or 400 Hz Rated
• Type 1 accuracy
• The CT primary current rating must exceed the maximum load current where they
are installed!

LCM