Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84776members
354220posts

MUX in FBD programs

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

Solved
otrotabi
Lieutenant
Lieutenant
0 Likes
2
383

MUX in FBD programs

I have not used Mux until recently, but I am starting to do it. It can save lots of time when used properly ! For example, in the project for multiple displays uploaded by Federico yesterday:

 

 

ProbeDisplayed := MUX(currentview,probeAI1,probeAI2, probeAI3,probeAI4,probeAI5);
dp := MUX(currentview,1,1,2,0,1);
um := MUX(currentView,5,5,3,1,5);	

/*	
	case currentview of 
	0:
			ProbeDisplayed := probeAI1;
			dp := 1; (* 1 decimal point *)
			um := 5; (* °C *)
	1:
			ProbeDisplayed := probeAI2;
			dp := 1; (* 1 decimal point *)
			um := 5; (* °C *)			
	2:			
			ProbeDisplayed := probeAI3;
			dp := 2; (* 2 decimal point *)
			um := 3; (* Bar *)

	3:			
			ProbeDisplayed := probeAI4;
			dp := 0; (* No decimal point *)
			um := 1; (* %Rh *)
	4:			
			ProbeDisplayed := probeAI5;
			dp := 1; (* 1 decimal point *)
			um := 5; (* °C *)
	end_case;
*/

 

 

However, in FBD I could not find a way to increase the number of inputs to the block. Is it possible somehow ? Default is 2 inputs.

 

FBDMUX.jpg


Accepted Solutions
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
378

Re: MUX in FBD programs

Click on the block and use increase pin from the toolbar

pin.PNG

 

See Answer In Context

Tags (3)
2 Replies 2
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
379

Re: MUX in FBD programs

Click on the block and use increase pin from the toolbar

pin.PNG

 

Tags (3)
otrotabi
Lieutenant
Lieutenant
0 Likes
0
372

Re: MUX in FBD programs

I see. I am so used to the right click procedure that works for other blocks that I did not notice that.  Thank you.

Tags (1)