Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84828members
354282posts

LMC058LF42 output faulty

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

VaughnKretzmann
Ensign
Ensign
0 Likes
1
376

LMC058LF42 output faulty

We have a customer who has a output faulty on the DO12TE output module on a LMC058LF42 controller.   Does the customer have to replace the entire controller or is it possible to just replace the DO12TE module?

Tags (1)
1 Reply 1
Ralf
Ensign Ensign
Ensign
0 Likes
0
367

Re: LMC058LF42 output faulty

Hello Vaughn,

 

unfortunately, it is not possibility to exchange a single “slice” of the LMC058 embedded IOs.

 

Best regards 

Ralf

Tags (1)