Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84599members
353865posts

BBMD configuration on M172P

Machine Automation Forum

A forum addressing machine automation solutions for the complete machine lifecycle. Including offers like Machine Advisor, Modicon PLC/PacDrive, Lexium or Preventa. Discuss and share knowledge on offers relating to cloud-based service platforms, machine localization and monitoring, industrial operations control, motion products as well as safety function!

sardila
Ensign
Ensign
0 Likes
2
210

BBMD configuration on M172P

Hi, 

 

I am currently implementing BACnet IP and BACnet MS/TP on M172p PLC. I couldn't find any documentation in regards BBMD configuration. 

 

At the moment I am using sysBACnet_BBMD block but it seems not working at all. 

 

Any ideas?? 

 

Thanks in advance 

Tags (1)
2 Replies 2
FedericoM
Lieutenant Lieutenant
Lieutenant
0 Likes
1
196

Re: BBMD configuration on M172P

Hi,

 

from M172 PICS: Device support registration as a foreign device

 

you can test doing something like that:

 

(* BBMD Service *)
(* IP 0.0.0.0 ==> BBMD disabled *)
xRet := sysBACnet_BBMD(BBMD_Ip1,BBMD_Ip2,BBMD_Ip3,BBMD_Ip4,BBMD_port,BBMD_tmo);

 

I suggest to check with a wireshark log.

 

Note that Bacnet IP and MS/TP can't be active at the same time.

 

Tags (1)
sardila
Ensign
Ensign
0 Likes
0
146

Re: BBMD configuration on M172P

Hi,

 

Thanks for your reply. I have implemented the block with the Ip address. Anything else is needed to configure BBMD ??

 

I am testing at the moment using YABE tool, but I don't have any BBMD device to test. I have a wireshark sniffer activated but obveously I cannot see any traffic through BBMD IP. 

 

I am using BACnet IP / YABE to test connectivity and everything is fine, however, I am not sure if my BBMD configuration is enough to establish connection between M172P and BBMD device due to lack of documentation.

 

Regards,

 

 

Tags (1)