Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84823members
354277posts

Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
MrPlant_Machine
Ensign
Ensign

Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Looking for options to achieve non-intrusive and near-zero latency cybersecurity of my petrochemical customer's plant industrial communications 


Accepted Solutions
G_Enigmedia
Ensign
Ensign

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Hi,

 

Enigmedia is specialized in securing communications with two main benefits: Non-intrusive installation and near zero latency. With Mercury you can get a secure communication using a somehow unsecure medium, even if the client or access point gets compromised by an attacker the data on air will be protected with encryption (impossible to recover or modify the original data), authentication (impossible to act as a rogue device), and accounting (traceability of activities).

 

Additionally, Mercury is completely transparent to the network and compatible with any device or protocol used in the network. Thanks to that, it does not require changing, or modifying, any existing IP configuration.

 

You can find more information about Mercury in the Exchange shop in this link.

 

Feel free to reach us for more information at contact@enigmediasecurity.com

 

Best,

See Answer In Context

5 Replies 5
G_Enigmedia
Ensign
Ensign

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Hi,

 

Enigmedia is specialized in securing communications with two main benefits: Non-intrusive installation and near zero latency. With Mercury you can get a secure communication using a somehow unsecure medium, even if the client or access point gets compromised by an attacker the data on air will be protected with encryption (impossible to recover or modify the original data), authentication (impossible to act as a rogue device), and accounting (traceability of activities).

 

Additionally, Mercury is completely transparent to the network and compatible with any device or protocol used in the network. Thanks to that, it does not require changing, or modifying, any existing IP configuration.

 

You can find more information about Mercury in the Exchange shop in this link.

 

Feel free to reach us for more information at contact@enigmediasecurity.com

 

Best,

iiot_consultant
Crewman
Crewman

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Cybersecurity needs a holistic view. If you are looking for a technology solution and not service, you could explore the following 5 options. They are listed inside the shop (right here on exchange): 

 

1/ Claroty: https://shop.exchange.se.com/apps/38661/claroty-platform#!overview 

 

2/ Waterfall security: https://shop.exchange.se.com/apps/39811/unidirectional-security-gateways#!overview 

 

3/ Extreme Networks: https://shop.exchange.se.com/apps/39231/extremecontrol#!overview 

 

4/ Tripwire: https://shop.exchange.se.com/apps/39621/tripwire-ics-security-suite#!overview

 

5/ Indegy: https://shop.exchange.se.com/apps/41315/indegy-industrial-cyber-security-suite#!overview 

 

 

Additionally, you could also explore the best practices at:

https://shop.exchange.se.com/apps/40125/reduce-vulnerability-to-cyber-attacks#!overview 

 

Hope it helps. Inbox me your specific requirements for a customized solution to your customer needs. 

MrPlant_Machine
Ensign
Ensign
1
3689

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Thanks. Lets take our discussion privately. I will inbox you. 

MrPlant_Machine
Ensign
Ensign

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Thank you for your response on options and best practices. I am sending you a message directly. 

G_Enigmedia
Ensign
Ensign
0 Likes
0
3674

Re: Urgent - Is it possible to cyber-secure a petrochemical plant industrial communications non-intrusively and with near-zero latency?

Hi,

 

Based on our direct message exchanges, thanks for accepting our product as solution to your customer needs,

 

Thanks and regards,