Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84428members
353626posts

On-demand update for M172 application on customer-side

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

S_Stolyarov
Lieutenant JG
Lieutenant JG
9
1580

On-demand update for M172 application on customer-side

Hi Everybody!

 

I want to rise a very interesting and complex topic about how to set up an on-demand application update process on customer-side for Controller M172 by digital instruments, remotely without service or engineering stuff.

 

For example, you are producing some range of products with PLC and found some bug in PLC application or want to give your customers new features.

 

One of the ideas that we have been thought about is to create internet resource where we can store application files, and the customer can register and see if the te any updates for installed machine and why. Then he can simply upload the files from the site and reload them to the controller via FTP.

 

Have you ever faced with such task and what are your thoughts on how this process can be set-up and what underwater rocks could be?

Tags (1)
9 Replies 9
Bastian_Schmitz
Commander Commander
Commander
3
1569

Re: On-demand update for M172 application on customer-side

The upload of the application (PLCIEC.COD) via FTP is possible. 

But if you upload only this file the EEPPROM values are missing. 

 

One of my customers has build up his own maintance tool for their service techincans. 

The upload the programm via FTP to controller.

After that the write all EEPROM and BIOS parameter via Modbus.

 

Please take care that the FTP function is in FW10 not working proper.

If you want test it use FW9 or wait till FW11. The problem will be fixed with the new Version.

Tags (2)
S_Stolyarov
Lieutenant JG
Lieutenant JG
0 Likes
2
1563

Re: On-demand update for M172 application on customer-side

Hi Bastian,

 

Thanks a lot! Do you know, if there any way to upload all values from the controller, maybe by the recipe, then replace an application and download values, again by recipe?

 

And I'm sorry, but what is FW9 or 10, is it firmware version?

Tags (1)
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
1562

Re: On-demand update for M172 application on customer-side

Hello,

You can use the target variable sysUsbCommand to get a solution like recipe.

For that You can upload via FTP to the NOR (Internal) or  MicroSD (if fitted) a text file based on the strucuter of the PARAM.RAW/DAT.

The value of 216 or 116 for target var sysUSBCommand shouldl be work. 

Please look into the proprties windows of the target variable to see how it works.

 

Regarding to the Firmware I mean actually we use the FW10 which means 668.10 (7-18IO) 596.10 (28-42IO).

The FTP function works proper with 668.9 or 596.9. 

But we have some problems in the actual version.

This problem will so far I know be fixed with the next Version of ESME HVAC. 

 

 

Tags (1)
S_Stolyarov
Lieutenant JG
Lieutenant JG
0 Likes
0
1560

Re: On-demand update for M172 application on customer-side

Thank you! We will try it when starting this project.

Tags (1)
S_Stolyarov
Lieutenant JG
Lieutenant JG
0 Likes
4
1551

Re: On-demand update for M172 application on customer-side

Dear colleagues!

 

Any other thoughts, ideas, how to organize PLC application updates via digital instruments, maybe modems, communication modules?

Tags (1)
Bastian_Schmitz
Commander Commander
Commander
0 Likes
3
1547

Re: On-demand update for M172 application on customer-side

If you use the RS232 communication plug in, you have the possibility to add a modem. 

I have personaly no expirence with such a solution.

 

If you have a Harmony HMI (like HMIST6xxx) or a HMIBSC in your solution you have additional the the possiblity to connect to the PLC via Secure Connect Advisor. This solution works very well. In that case you can update the PLC via the software via remot, and you have the possibilty to check the webvisualisation of the PLC via Mobil Device via secure Connect advisor.

 

S_Stolyarov
Lieutenant JG
Lieutenant JG
0 Likes
2
1522

Re: On-demand update for M172 application on customer-side

Thank you!

 

Have anyone have experience with updating PLC application via modem, connected to RS232?

Tags (1)
Bastian_Schmitz
Commander Commander
Commander
0 Likes
1
1393

Re: On-demand update for M172 application on customer-side

Sorry but I have personaly now expirence with the use of a modem together with TM17x. 

But if you look in the catalog then the possibility download a program via Modem is defined.

 

You can find the actual catalog here

Catalog TM17x

 

3.PNG

Tags (1)
S_Stolyarov
Lieutenant JG
Lieutenant JG
0 Likes
0
1342

Re: On-demand update for M172 application on customer-side

Aha,

 

Thank you, we'll try this possibility when we get to this!

Tags (1)