Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84583members
353850posts

NEW VERSION AVAILABLE: Unity Developer's Edition (UDE).

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Rodrigo_Garcia
Administrator Administrator
Administrator

NEW VERSION AVAILABLE: Unity Developer's Edition (UDE).


Discover the new version of Unity Developer's Edition (UDE)!

 

Unity Developer’s Edition allows to develop client applications that access automation projects via interfaces provided by various servers. Client applications can be written in any programming language that is supported by the component object model (COM) Visual-Basic, Visual C++ or Visual Basic Application (VBA).

 

The projects, data and objects are thus made accesible to external tools.

 

A UDE client application may access the automation servers by either of two methods:

  • dynamic access, via a COM or a distributed (DCOM) interface
  • static access, by way of XML data exchanges

 

This UDE Update V14 provides the content of the last UDE release (version 2.1), with additional updates that came with Control Expert V14 and V14.1

Rodrigo G. 


Industrial Automation Community manager

Tags (2)
1 Reply 1
Omaelk
Administrator Administrator
Administrator
0 Likes
0
521

Re: NEW VERSION AVAILABLE: Unity Developer's Edition (UDE).

thanks for sharing 🙂

 

Tags (1)