Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84846members
354304posts

NEW: Discover the release of EcoStruxure Machine Expert - HVAC v1.2.1

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Rodrigo_Garcia
Administrator Administrator
Administrator

NEW: Discover the release of EcoStruxure Machine Expert - HVAC v1.2.1

The new version of the Modicon M171/M172 programming software introduces several improvements in particular related to cybersecurity in accordance to Schneider Electric global strategy.

 

Improved cybersecurity

Implementation of cybersecurity best practices adoption to force user to change web password at first access and manage the unsecure protocols Modbus/TCP, FTP and Bacnet now disabled by default.

 

Improved programming experience with more functionalities:

  • Target Real Time Clock alignment during Download All
  • Variable export functions for Schneider Electric HMI programming software Ecostruxure Operator Machine Expert
  • Live debug function for ST language
  • Support for direct bit access
  • Optimization of watch windows
  • Support for dynamic array bound using a symbolic constant
  • POU can be saved into separate files to facilitate the integration with version control systems
  • Zoom function in Programming Editor

 

Firmware updates:

New features in Modicon M172 (Firmware Msk 596.10 and Msk 668.10)

  • Increased number of Modbus TCP Client from 3 to 8
  • Modbus TCP / BACnet IP / FTP are disabled by default which need therefore to be manually enabled.
  • Increased number of registers from 16 to 20 for the following Modbus on event functions
  • Introduced new Target variables to count the number of Modbus message received on the related serial port
  • Improvement of sysUART Target functions

 

New features in TM171VEV EEVD valve driver (Firmware Msk 589.20)

  • Implemented Unipolar Valves driving for Parker-Sporlan CEV models
  •  

>>>> DOWNLOAD THE SOFTWARE FOR FREE!!! <<<< 

 

 

 

Rodrigo G. 


Industrial Automation Community manager

Tags (1)