Industrial Edge Computing Forum
Partnering with Schneider Electric for edge computing empowers System Integrators to differentiate and grow their business in today’s IIoT world through an expanded offer portfolio, essential training, risk reduction, and reduced time to market.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2021-08-06 01:57 AM
The benefits of industrial edge computing are becoming more apparent across a variety of industries. It brings low-latency compute capacity closer to applications and in the process, makes real-time data processing faster. Yet, building an edge computing solution can take a lot of work.
If you’re manufacturing goods in a factory or producing safe water or clean power in a facility, you would start by designing an architecture that uses edge computing platforms loaded with the best software you can find for monitoring and control. By installing data collection on-premise at the edge, you also eliminate bandwidth and latency issues as information is transmitted to the enterprise and cloud.
The whole process is long and involved, requiring a fair amount of research and consultation to ensure the best possible combination of IT and OT components. In addition, you are likely to communicate with multiple technology providers and distributors just to put a plan together.
There is a better way. It involves deploying a pre-configured, pre-validated hyperconverged infrastructure micro data center (MDC) that combines all the necessary components. This approach includes software pre-installed in a redundant and cybersecure edge computing platform, networking hardware, and power management via a Smart-UPSTM. This solution can accelerate industrial edge deployments by reducing field engineering time by 40%, with 20% faster time to market and 7% lower maintenance costs.
But who puts it all together?
Schneider Electric has a partnership with Stratus Technologies to deliver end-to-end edge computing solutions. Stratus is all about downtime prevention and workload consolidation. It does this by delivering scalable, flexible, and operationally resilient systems with built-in redundancy and virtualization that comes in a single, integrated, edge computing platform. John Knorr, VP of Global IT Alliances at Schneider Electric, said, “When partnering with Stratus, we spoke about the many day-to-day responsibilities of a System Integrator and the security and privacy concerns raised with outsourcing IT. We made it our mission to not only bridge the gap of IT and OT but simplify the purchase, deployment, and management cycle all together with a one-stop-shop solution.”
A third partner, AVEVA, provides the industrial operations software, leveraging reference designs that specify the components and configuration needed for quick deployment at the edge. Reference designs map out the needs of industrial edge installations, so you don’t have to be an IT expert.
Avnet, a global distributor and solutions provider, brings all the components together. Avnet provides a one-stop shop for end customers, integrators, and OT distributors to order a complete, integrated turnkey solution. Each solution starts with a standardized offering approved and validated by the manufacturing partners. As Avnet builds the MDC, an integration partner works on customizing the virtual machines (VM) that are later integrated into the overall solution.
Bringing decades of experience in the IT and OT markets to each project, Avnet takes the complicated work of doing the build-out off the customer’s internal engineering teams, enabling them to focus on their key competencies.
Avnet also is able to provide a project estimate much earlier in the process than if you were putting together the solution on your own. Estimates usually fall within plus or minus 10% of the final cost. Getting the estimate early helps move along the project.
Leveraging the Schneider partnership with Stratus, AVEVA and Avnet makes for a much more streamlined and simplified journey, whether you’re an end-user or system integrator. If you’re the end customer, you need only deal with one company, as opposed to four or five.
Avnet is involved through the entire process, even handling the Factory Acceptance Test (FAT) remotely to ensure a solution is built to spec. Post-implementation, customers can opt to keep Avnet involved by managing and maintaining the environment.
Learn more about how to leverage hyperconverged micro data center solutions. Coming soon, Avnet will launch a digital portal where you can review a solutions catalogue, get quotes, and place orders.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.