Issue
A device inadvertently left in Operator Mode after a maintenance activity ignores the commands coming from the automation application. The process then cannot resume normal operation automatically, which can lead to unexpected production downtime and require additional operator intervention.
The issue is even more significant in distributed automation applications, where the orchestration layer and the controlled equipment may be geographically separated: large facilities, remote utility areas, mining operations, water treatment plants or multi-site architectures. In these cases the distance between the Control Command and the Controllers makes physical intervention slow and costly.
Resolution
This article shows how IEC 61499 logic can force the transition from Operator Mode to Program Local or Program Remote. Integrated into the control strategy, this lets the system recover from an incorrect operating mode and restore normal operation without any local operator action.
The approach applies to control modules based on the SE.App2CommonProcess library and can be included in automated startup or recovery to improve availability.
Disclaimer
The views and opinions expressed in this article are those of the author(s) and do not necessarily reflect the official policy or position of Schneider Electric.