Issue
There are two in-rack Ethernet communication modules that allow the integration of Modicon Edge I/O NTS in M340 systems. But only one of them, the BMXNOC0401, enables such an integration through EtherNet/IP communication.
Resolution
This article provides a step-by-step guide on how to integrate a Modicon Edge I/O NTS island in an M340 architecture through EtherNet/IP communication using the BMXNOC0401 module.
.
Disclaimer
The views and opinions expressed in this article are those of the author(s) and do not necessarily reflect the official policy or position of Schneider Electric.