Issue
The purpose of this article is to introduce the necessary steps to configure a station in a Lexium™ MC12 Multicarrier application of EcoStruxure Machine Expert via Python Script. It explains in detail how a new station can be added to the application using the provided script. The following sections describe the script workflow, the generated project modifications, and the required parameters for successful station creation.
Resolution
This article has highlighted how a new station can be added to the reference project using the provided Python script. The script automates the required project modifications and significantly reduces manual engineering effort. After execution, only a few application-specific settings, such as station parameters, target stations, visualization, and station logic, need to be reviewed and adapted. This approach provides a fast and efficient way to extend the application with additional stations.