Issue
In a multi-core system such as Modicon M660, performance issues such as uneven CPU load distribution, jitter in cyclic tasks or unexpected task interference may occur when all tasks are executed on the same CPU core by default.
Resolution
To improve task scheduling, optimize performance and reduce interference, EcoStruxure Machine Expert allows assigning task group to specific CPU core.
Disclaimer
The views and opinions expressed in this article are those of the author(s) and do not necessarily reflect the official policy or position of Schneider Electric.