Issue
Validate the behavior of a function block connected to I/O (inputs/outputs) without physical hardware, avoiding the limitations of direct forcing of variables and ad‑hoc simulation functions.
Resolution
Implement virtual input/output modules as HW CATs (Hardware Composite Automation Types). These HW CATs act as a software simulation interface between the function block and the HMI.
The attached ZIP file contains all the FB files as well as the solution used to create the document.
Disclaimer
The views and opinions expressed in this article are those of the author(s) and do not necessarily reflect the official policy or position of Schneider Electric.