Issue
With the introduction of EcoStruxure Automation Expert Version 25.0, users can synchronize templates from AVEVA System Platform by filtering and selecting the appropriate template.
AVEVA System Platform can contain templates whose attributes can be imported into EcoStruxure Automation Expert and used within a Composite Automation Type (CAT). To import these templates, you must run the Sync AVEVA SP Templates process
When running this process for the first time, some default templates may require updating.
Resolution
This document contains trick and tips for updating the Templates
Disclaimer
The views and opinions expressed in this article are those of the author(s) and do not necessarily reflect the official policy or position of Schneider Electric.