Objective
This article explains the setup and optimization of control loop parameters for a Lexium™ MC12 Multi Carrier application. It provides an overview of the available controller parameters, their influence on system behavior, and a recommended tuning procedure for achieving stable and accurate carrier motion.
By following the recommended workflow, users can systematically optimize the velocity and position control loops to achieve the desired dynamics, positioning accuracy, and overall system stability.
Resolution
This article highlights the key aspects of configuring and tuning the Control Loop Parameters for a Lexium™ MC12 Multicarrier application. It explains the purpose and effect of the main controller parameters, including carrier mass, velocity controller gains, and position controller gains, and provides guidance for achieving stable and accurate carrier motion.