How to perform X-way test for Unitelway connection
Industrial Automation How-to videos
How-to videos on Schneider Electric Industrial Automation products and solutions. In general, these videos help provide a clear demonstration on the best method to accomplish a given task.
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
Showing results for
Show only
|
Search instead for
Did you mean:
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
1. Is there's instruction to learn how to make the configurations for Unitelway connection?! Reply: Refer the attached communication driver manual from below link to learn the Unitelway configuration and others.
2. Also can i connect to PL74823A, without installing its SRAM memory card?
reply: Yes, PLC can be connected with CPU terminal port over Unitelway connection with no dependency on SRAM Memory Card. Impact of memory card will be on Application program not on CPU connection.
3. Also if the memory card batteries is empty, it will make problem in the connection or not?
Reply: Yes, PLC can be connected with CPU terminal port over Unitelway connection if the memory card batteries is empty. Impact of memory card will be on Application program not on CPU connection.
4. And if i have a new SRAM Memory card, can I connect through the Default IP Address?
Reply: Yes, if there is no application code inside the CPU containing IP address. Refer below FAQ to extract default IP from MAC address.