Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

"Type mismatch in assignment" of a constant structure

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • Re: "Type mismatch in assignment" of a constant structure
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to HVAC and Pumping Forum
Start a Topic
Solved
obscuresc
obscuresc
Troubleshooter

Posted: ‎2022-03-03 08:34 PM

0 Likes
2
3076
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
Posted: ‎2022-03-03 08:34 PM

"Type mismatch in assignment" of a constant structure

Hi,

 

Per above, I am received an error G0101 for "Type mismatch in assignment".

I have created a constant structure that I use for state control.

I use it in place of an enumeration because of it's ability to capture type within the structure.

 

Below is an example of a struct I was able to reproduce the error upon.

 

 

TestStruct_t: STRUCT
	item0 : USINT := 0;
	item1 : USINT := 1;
	item2 : USINT := 2;
END_STRUCT;

 

 

I instantiate it so that it may be used. Note that because it is a constant, I have to initialise the members.

 

VAR_GLOBAL
	cnt : INT;
	usiTestAssignment : USINT;
END_VAR

VAR_GLOBAL CONSTANT
	AConstStruct : TestStruct_t := (item0 := 0, item1 := 1, item2 := 2);
END_VAR

 

 

Upon use for an assignment

 

usiTestAssignment := AConstStruct.item0;

 

the following error results

 

MAIN(3) - error G0101:  USITESTASSIGNMENT => Type mismatch in assignment

 

 

As far as I can tell, both 'usiTestAssignment' and 'AConstStruct.item0' are of the same type.

I can resolve this issue by doing change to the line below, instead of using the previous assignment, but this defeats sort of defeats the purpose for using the constant structure in the first place.

 

usiTestAssignment := AConstStruct.item0 + TO_USINT(0);

 

 

How can I resolve this issue without having to use the 'hack' of 'TO_USINT(0)'?

Thanks.

Labels
  • Labels:
  • HVAC
  • Tags:
  • Ecostruxure HVAC
  • english
  • TM172
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Bastian_Schmitz
Bastian_Schmitz Champion
Champion

Posted: ‎2022-03-03 10:53 PM

0 Likes
1
3063
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
Posted: ‎2022-03-03 10:53 PM

The problem are the inital values together with the attribut constant on a struct.

If you did not use the attribut constant you don´t need to define in the declaration of the variabele a init value.

If you declare the variable in this way it works proper.

At the moment I did not understand the purpose to use attribut of constant in this behaivor.

 

best regards

 

See Answer In Context

  • Tags:
  • english
  • ESME HVAC
  • M172
Reply

Link copied. Please paste this link to share this article on your social media post.

Replies 2
Bastian_Schmitz
Bastian_Schmitz Champion
Champion

Posted: ‎2022-03-03 10:53 PM

0 Likes
1
3064
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
Posted: ‎2022-03-03 10:53 PM

The problem are the inital values together with the attribut constant on a struct.

If you did not use the attribut constant you don´t need to define in the declaration of the variabele a init value.

If you declare the variable in this way it works proper.

At the moment I did not understand the purpose to use attribut of constant in this behaivor.

 

best regards

 

  • Tags:
  • english
  • ESME HVAC
  • M172
Reply

Link copied. Please paste this link to share this article on your social media post.

obscuresc
obscuresc
Troubleshooter

Posted: ‎2022-03-06 03:05 PM

In response to Bastian_Schmitz
0 Likes
0
3012
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
Posted: ‎2022-03-06 03:05 PM

Hi @Bastian_Schmitz 

 

I'm using constant on a struct to approximate the functionality of a typed enum like in C/C++.

When creating an enum in IEC, I don't seem to have the ability to set its type, and hence when using it, I have type cast every instance of the enum to prevent compiler warnings.

 

My alternative to use a struct to specify the type, and use const keyword, to prevent accidental overwrite of members in the struct.

 

I'll remove const, but I feel like the compiler should be able to handle it in this instance.

 

Thanks,

Jack
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.