Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Simulation Testing Between EcoStruxure Machine Expert-HVAC and Vijeo Designer Basic

HVAC and Pumping Forum

Support Forum for HVAC and pumping machines, Modicon M17x and EcoStruxure Machine Expert HVAC software for chillers, AHU, CRAC units for datacenters or process chillers applications - from design, implementation to troubleshooting and more, by Schneider Electric.
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
  • Industrial Automation
  • HVAC and Pumping Forum
  • Simulation Testing Between EcoStruxure Machine Expert-HVAC and Vijeo Designer Basic
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
FedericoM
FedericoM Mentor
119
Bastian_Schmitz
Bastian_Schmitz Champion
64
M_Cervati
M_Cervati Troubleshooter
18
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to HVAC and Pumping Forum
Start a Topic
Solved
Saad_Nazeer
Saad_Nazeer
Contributor

Posted: ‎2026-01-20 01:43 AM . Last Modified: ‎2026-01-20 01:44 AM

0 Likes
1
291
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
Posted: ‎2026-01-20 01:43 AM . Last Modified: ‎2026-01-20 01:44 AM

Simulation Testing Between EcoStruxure Machine Expert-HVAC and Vijeo Designer Basic

Is it possible to perform simulation testing between EcoStruxure Machine Expert-HVAC and Vijeo Designer Basic? Specifically, can Vijeo Designer Basic be used to simulate or test HMI interaction with an EcoStruxure Machine Expert-HVAC application?

Labels
  • Labels:
  • HVAC
  • Tags:
  • EcoStruxure Machine Expert-HVAC
  • english
  • Vijeo Designer Basic
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
ismailozinan
ismailozinan Leader
Leader

Posted: ‎2026-01-20 09:23 PM . Last Modified: ‎2026-01-20 09:35 PM

0 Likes
0
282
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
Posted: ‎2026-01-20 09:23 PM . Last Modified: ‎2026-01-20 09:35 PM

Hello,

Without the physical device(TM172), it is unfortunately not possible to run the HVAC software in simulation mode using a Basic HMI.

if there is physical device(TM172) answer is YES . Using a Basic or any other HMI, you can achieve this without a physical HMI, by using an HMI software running on Windows in simulation mode.

If M172 Modbus TCP will be used:
After completing the TCP configuration, you can control the real M172 device from the HMI software simulation by configuring the HMI side as a Client.

If M172 Modbus RTU (RS485) will be used:
In this case, the HMI side must be configured as Master. This allows the real M172 device to be controlled from the HMI software simulation.

If you will perform Modbus RTU (RS485) simulation:
The RS485 converter connected to the PC must be configured as COM2 via Windows > Device Manager. This is required because, on a real HMI, the RS485 communication is performed through the COM2 port, and the simulation must behave in the same way.

For Modbus TCP simulation over IP:
When you ping the TM172, it must be reachable, and port 15797 must be configured in advance via USB cable, web browser, or ESME HVAC software.

You can see an example simulation in the video provided at the link .

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
ismailozinan
ismailozinan Leader
Leader

Posted: ‎2026-01-20 09:23 PM . Last Modified: ‎2026-01-20 09:35 PM

0 Likes
0
283
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
Posted: ‎2026-01-20 09:23 PM . Last Modified: ‎2026-01-20 09:35 PM

Hello,

Without the physical device(TM172), it is unfortunately not possible to run the HVAC software in simulation mode using a Basic HMI.

if there is physical device(TM172) answer is YES . Using a Basic or any other HMI, you can achieve this without a physical HMI, by using an HMI software running on Windows in simulation mode.

If M172 Modbus TCP will be used:
After completing the TCP configuration, you can control the real M172 device from the HMI software simulation by configuring the HMI side as a Client.

If M172 Modbus RTU (RS485) will be used:
In this case, the HMI side must be configured as Master. This allows the real M172 device to be controlled from the HMI software simulation.

If you will perform Modbus RTU (RS485) simulation:
The RS485 converter connected to the PC must be configured as COM2 via Windows > Device Manager. This is required because, on a real HMI, the RS485 communication is performed through the COM2 port, and the simulation must behave in the same way.

For Modbus TCP simulation over IP:
When you ping the TM172, it must be reachable, and port 15797 must be configured in advance via USB cable, web browser, or ESME HVAC software.

You can see an example simulation in the video provided at the link .
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.