Geo SCADA Knowledge Base
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Originally published on Geo SCADA Knowledge Base by sbeadle1 | June 10, 2021 04:20 AM
📖 Home
It is important to apply Microsoft Windows updates to keep systems secure. Occasionally there will be incompatibility issues noted here. Please check back regularly for updates.
Microsoft provides the Windows Update Service that securely distributes updates and bug fixes in the form of patches. Microsoft schedules the release of patches via Windows Update.
To provide customers the confidence that they can install Microsoft patches without adversely affecting existing installations of Geo SCADA Expert, a set of regression tests are run on currently supported Geo SCADA Expert versions and their supported server and workstation Microsoft Windows Operating System versions. These regression tests are run on the newly-released Windows patches monthly, with the results published on this page for reference once they are released.
The results documentation is cumulative, meaning that the results from the current month's testing are added to the results of the previous month, and so forth. As a result it is only necessary to review the current month's results spreadsheet to get a comprehensive understanding of the testing performed in the current calendar year. Testing results are archived annually, with previous years' results available below for reference.
Any testing is performed using all the approved previous months of patches installed, except where a more recent patch supersedes that earlier patch.
Any out-of-band (unscheduled) patch released by Microsoft is not tested until the next scheduled patches are released, at which point the out-of-band patch will be tested alongside the scheduled patches.
Microsoft Windows Server, Workstation, .NET and Internet Explorer security and general updates are tested including default services such as Windows Defender, any other Microsoft products such as Microsoft Office are not included within the approval testing.
Third party patches such as those provided by SAP (Crystal Reports Editor), Oracle (Java) and Adobe (Reader) are not included within the testing.
Incompatibility Warning |
Added 30 Jan 2023 |
Operating Systems | Windows Server 2022, 2019, 2016 and 2012 R2. Windows 11 and Windows 10. |
Geo SCADA Versions | Geo SCADA 2022 Initial Release |
Parts of Geo SCADA Affected | Installation of OPC UA Server Prerequisites |
Specific Patches | Windows Server 2022: KB5020877 – December 13, 2022 Cumulative Update for .NET Framework 3.5 and 4.8 (no January 2023 version available) Windows Server 2019: KB5020874 – December 13, 2022 Cumulative Update for .NET Framework 3.5 and 4.8 (no January 2023 version available) Windows Server 2016: KB5020873 – December 13, 2022 Cumulative Update for .NET Framework 4.8 (no January 2023 version available) Windows Server 2012 R2: KB5020878 – December 13, 2022 Security and Quality Rollup for .NET Framework 4.8 (no January 2023 version available) Windows 11: KB5020875 – December 13, 2022 Cumulative Update for .NET Framework 3.5 and 4.8 Windows 11: KB5022407 – January 19, 2023 Cumulative Update for .NET Framework 3.5, and 4.8 Windows 10: KB5020872 – December 13, 2022 Cumulative Update for .NET Framework 3.5 and 4.8 Windows 10: KB5022405 – January 19, 2023 Cumulative Update Preview for .NET Framework 3.5 and 4.8 |
Symptoms | Failure to install the Aveva PCS Prerequisites for OPC UA Server. There is no problem if these Prerequisites are not chosen. |
Mitigation | Microsoft have recognised that their update has caused a problem. They have provided a workaround in the following link: https://support.microsoft.com/en-gb/topic/kb5022083-change-in-how-wpf-based-applications-render-xps-... We confirm that the Microsoft workaround resolves the issue until a future Microsoft update removes the need to use it.
Without the workaround, if the OPC UA Server is required please install Geo SCADA 2022 before installing the above Windows updates (or future patch rollups containing this same update). AVEVA is also working to resolve this in the installer, which may be included in a Monthly Update to Geo SCADA 2022. Please check back here for updates. |
Resolved by | Microsoft Updates for .Net Framework for February 2023 |
Incompatibility Warning |
Added 3 Nov 2022, Updated 6 Jan 2023 and 30 Jan 2023 |
Operating Systems | Windows 10, 11, Server 2012 R2, Server 2016, Server 2019 and Server 2022 |
Geo SCADA Versions | Geo SCADA 2021 |
Parts of Geo SCADA Affected | ViewX Client |
Specific Patches | 2022-10 Cumulative Update for .NET Framework 3.5, 4.8 and 4.8.1 for Windows 10 Version 21H2 (KB5018545) 2022-10 Cumulative Update for .NET Framework 3.5, 4.8 and 4.8.1 for Windows 10 Version 21H1 (KB5018544) 2022-10 Cumulative Update for .NET Framework 3.5, 4.8 and 4.8.1 for Windows 11 (KB5018546) 2022-10 Security and Quality Rollup for .NET Framework 3.5, 4.6.2, 4.7, 4.7.1, 4.7.2, 4.8 for Windows 8.1, RT 8.1, and Windows Server 2012 R2 (KB5018549) 2022-10 Cumulative Update for .NET Framework 4.8 for Windows 10, version 1607 and Windows Server 2016 (KB5018515) 2022-10 Cumulative Update for .NET Framework 3.5, 4.7.2 and 4.8 for Windows 10, version 1809 and Windows Server 2019 (KB5018542) 2022-10 Cumulative Update for .NET Framework 3.5, 4.8 and 4.8.1 for Microsoft server operating system version 21H2 (KB5018551) |
Symptoms | If the user uses the 'Locate in Database' option from a list and then logs out of ViewX, ViewX will crash and a minidump will be generated. The Windows Update changes are known to affect applications using the Actipro tree list control, used by the ViewX database tree. |
Mitigation | a) Do not install this update (or future patch rollups containing this same update) until either: i) You have installed the Microsoft December 2022 rollup updates. ii) You have installed the Geo SCADA update issued in December 2022. b) There is a workaround from Microsoft. Add this line to the file SE.SCADA.ViewX.exe.config file in Program Files (x86). (Place the line before the existing text </runtime>): <AppContextSwitchOverrides value= "Switch.System.Windows.Controls.VirtualizingStackPanel.OptOutOfCollectionChangeFix=true"/> </runtime> |
Resolved by | Microsoft Updates for .Net Framework for February 2023 |
Incompatibility Warning |
Added 27 June 2022, Updated 6 Jan 2023 |
Operating Systems | Windows Server 2019 |
Geo SCADA Versions | Geo SCADA 2019, 2020 and 2021, except 2022 and 2021 from December 2022 |
Parts of Geo SCADA Affected | Virtual ViewX Server |
Specific Patches | 2022-06 Cumulative Update for Windows Server 2019 for x64-based Systems (KB5014692) |
Symptoms | Only one user will be permitted to log in to Virtual ViewX |
Mitigation |
Do not install this update (or future patch rollups containing this same update) until you have installed the December 2022 update of Geo SCADA 2021, or Geo SCADA 2022. |
Resolved by | December 2022 update of Geo SCADA 2021, or Geo SCADA 2022 |
The latest Patch Tests were carried out in May 2023 with the results available for download below.
It is anticipated that the results of the next round of Microsoft patch testing will be published here after June 27th 2023.
Schneider Electric recommends that this released patch information is used alongside a suitable patch management process, for example as documented in IEC-62443-2-3, which includes additional local testing using customer specific configuration prior to deployment to any production system.
Test results are archived annually. The previous results are available below. Generally use the latest file which rolls up previous months. Annual files are listed too. The December 2022 file includes test results from 2021 & 2020.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.