New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Geo SCADA 2025 R2 Operating System Support
Geo SCADA Knowledge Base
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
Showing results for
Show only
|
Search instead for
Did you mean:
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
HomeBack It is strongly recommended that systems running on server hardware need to use the Windows Server operating system. Server operating systems are designed for servicing entire systems rather than individual computers or small networks and so are better suited for larger SCADA Server or Web Server systems with more than two clients.
Systems running on desktop hardware should run desktop operating systems such as Windows 11. Desktop operating systems are designed for user interaction on the computer on which they are installed.
Desktop operating systems should not be used for SCADA Servers or Web Servers with more than two clients as the TCP/IP security measures in these operating systems can cause significant delays.
Refer to the following table for supported Operating System versions:
64-Bit Operating Systems
(ViewX client, SCADA Server and Web Server)
Desktop Hardware
Windows 11 Professional and Enterprise editions
Windows 11 IoT Enterprise edition
Geo SCADA 2025 R2 is not directly supported on Windows 10, the last tested updates will be for October 2026.
Server Hardware
Windows Server 2025 (Standard and Datacenter editions) Windows Server 2022 (Standard and Datacenter editions) Windows Server 2019 (Standard and Datacenter editions)
Use of Geo SCADA WebX requires Internet Explorer 11 for web-based operation which has been obsoleted by Microsoft. You may be able to use Edge in 'IE Mode' for WebX. For Web use we recommend the Virtual ViewX User Interface which is accessible from any up-to-date HTML5 browser on various types of desktop, laptop, tablet or large format phone.