Geo SCADA Knowledge Base
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Originally published on Geo SCADA Knowledge Base by sbeadle | January 09, 2023 11:46 AM
Upgrading from Geo SCADA Expert 2021
Upgrading from Geo SCADA Expert 2020
Upgrading from Geo SCADA Expert 2019
Upgrading from ClearSCADA 2017 R3
Upgrading from ClearSCADA 2017 R1 and R2 Prior to June 2018
* Please be aware of all the issues covered in the above sections in addition to the following.*
An example XML file for the June 2018 update onwards is shown in the 2020 Upgrade Notes page
Upgrading ClearSCADA Mobile
Between ClearSCADA 2017 and ClearSCADA 2017 R2 the location of the Mobile Settings database changed.
Therefore upgrading from a version of ClearSCADA Mobile at or before ClearSCADA 2017 will require your action.
You will need to move your database (.sdf file) from:
C:\ProgramData\Schneider Electric\ClearSCADA Mobile
to
C:\ProgramData\Schneider Electric\ClearSCADA
Upgrading from ClearSCADA 2015 R2.x
* Please be aware of all the issues covered in the above sections in addition to the following.*
Upgrading from ClearSCADA 2015 R1.x
Please be aware of all the issues covered in the above sections in addition to the following.
The installation of Geo SCADA Mobile and Virtual ViewX is separate in Geo SCADA Expert 2019 to provide a simplified upgrade experience. If required the Virtual ViewX installation will be executed after successful installation of Geo SCADA 2019, whereas the installation of Geo SCADA Mobile will need to be manually executed if required via the link on the Geo SCADA installation splash screen.
Existing installations of ClearSCADA 2015 R1 Web and Mobile will first need to be uninstalled prior to installation of ClearSCADA 2015 R2. The re-installation of Virtual ViewX to replace WebX after installation of ClearSCADA 2015 R2 will need to manually re-configure any non-default ports, as these will not be remembered from the previous WebX installation. Mobile users running versions prior to ClearSCADA 2015 R1 should be able to upgrade to Geo SCADA Expert 2019 without first uninstalling ClearSCADA Mobile.
For example, an upgrade from ClearSCADA 2013 R1.2 (73.4955) to ClearSCADA 2013 R2 (74.5094) is valid because 5094 > 4955. In comparison, an upgrade from ClearSCADA 2013 R2.2 (74.5700) to ClearSCADA 2014 R1 (75.5210) is not recommended because 5210 < 5700, even though it is an increase in the minor version number, as this may reintroduce bugs that have been fixed in the later version.
ClearSCADA should only be upgraded to a newer version that has a higher build number than the currently installed version.
Upgrading from ClearSCADA 2014 R1.x
Please be aware of all the issues covered in the above sections in addition to the following.
Upgrading from ClearSCADA 2013 R2.x
Please be aware of all the issues covered in the above sections in addition to the following.
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.