New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Access vast amounts of technical know-how and pro tips from our community of Geo SCADA experts.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Originally published on Geo SCADA Knowledge Base by sbeadle | January 26, 2026 01:19 PM
These samples are .sde files for importing into Geo SCADA. They include special symbols and performance monitoring.
Also see:
Driver Development Kit Driver Examples
It is useful to see the status of multiple servers on mimics.
This is a large configuration sample which contains server state and performance gathering setup to show the synchronization status of multiple servers together with other performance data. See the configuration .sde below named ''System - Server Status Mon Setup (2022) V3.sde". It has been saved with the 2022 format so that you can use it with older systems. There is a setup guide in the document "System - Server Status Mon Setup.docx".
A radar graph shows several variables as a polygon, enabling an operator to see quickly the health of a process. This folder contains a series of radar graph mimics suitable for embedding. A simple and an advanced version of each is included, with the advanced version containing alarm limits, colored markers and a shadow to show previous values. There are named parameters for each mimic. An example is included to demonstrate how they are used.
Download and find attached at the bottom of the page "Radar Graphs.sde"
This configuration brings out the overall system loading figures into individual points. Figures such as point processed, historic values stored, events stored etc. Suitable for ClearSCADA 2015 R2 onwards.
Processes figures every minute, but the interval can be altered by changing the Logic execution interval.
Download and find attached at the bottom of the page "Performance Stats.sde"
This file is a demonstration of advanced ClearSCADA mimic scripting.
Download and find attached at the bottom of the page "SameGame.sde"
It is possible, by use of symbol/mimic design and script, to create mimics which can be switched to a Playback mode using on-screen controls to pause, change time and move forwards or back in time. To do this you need to design mimic symbols with a separate playback layer and animate the symbols with historic data and a user registry key to represent the time the user wants to see data for. Naturally the historic data feature must be active for any data sources using this method. Please see the file below 'PlaybackSample.sde'. This sample contains an embedded mimic with parameters, indirect animations for time offset and the selections for historic data. Please inspect this sample carefully to consider if using this technique is appropriate for your system.
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.