Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84723members
354130posts

Upgrade Com'X 210 to Panel Server Universal

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Solved
Diego_Ramirez
Ensign
Ensign
0 Likes
3
455

Upgrade Com'X 210 to Panel Server Universal

Hi,

 

I'm using Com'X210 to periodically send energy data in CSV files to FTP server for my 3rd party energy management system. 

 

Will I need to change anything in my setup when I replace Com'X with Panel Server Universal?

 

Thanks for guidance

Diego​

Tags (1)

Accepted Solutions
Randi_Dolan
Commander Commander
Commander

Re: Upgrade Com'X 210 to Panel Server Universal

Hi Diego,

 

Currently, the Panel Server doesn't support data file export via FTP.  Data can either be manually exported or exported to a Schneider Electric cloud application.

 

However, the Panel Server will support SFTP data export in an upcoming release.  When this happens, you will have to configure your server to use SFTP instead of FTP.

 

I hope this help.

Randi

See Answer In Context

Tags (1)
3 Replies 3
Randi_Dolan
Commander Commander
Commander

Re: Upgrade Com'X 210 to Panel Server Universal

Hi Diego,

 

Currently, the Panel Server doesn't support data file export via FTP.  Data can either be manually exported or exported to a Schneider Electric cloud application.

 

However, the Panel Server will support SFTP data export in an upcoming release.  When this happens, you will have to configure your server to use SFTP instead of FTP.

 

I hope this help.

Randi

Tags (1)
sesa157458_brid
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
1
438

Re: Upgrade Com'X 210 to Panel Server Universal

Hello @Randi_Dolan,

 

Do we have a spec of the csv format to be used by PAS ?

 

Kind Regards

Tags (1)
Szymon_Hochół
Commander Commander
Commander
0 Likes
0
424

Re: Upgrade Com'X 210 to Panel Server Universal

Hi @sesa157458_brid,

the CSV format is not officially available yet. However, some changes in the CSV file structure are likely to be introduced vs. what was generated by Com'X.

 

Best regards

Tags (1)