Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84375members
353559posts

Problems with boolean registers in Com'X

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Daniel_Borle
Commander Commander
Commander
0 Likes
2
153

Problems with boolean registers in Com'X

Hi,

I wrote a driver for the implementation of an I/O-module in the Com'X510. Now I found the following problems:

1. The names that I've used for the different Inputs are showed on the Device Settings page as element_ plus the Name I gave them in the driver and they are in alphabetical order instead of the order I programmed them in the driver:

Driver:

Device Settings:

2. It's not possible to see this device on the Monitoring or on the Measurement Table page.

Are these bugs or did I made a wrong manipulation?

Thanks

Daniel

2 Replies 2
Colton_Peltier
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
1
124

Re: Problems with boolean registers in Com'X

Hi Daniel,

Can you attach an export of the custom model you're using?

Best,

Colton

Daniel_Borle
Commander Commander
Commander
0 Likes
0
124

Re: Problems with boolean registers in Com'X

Hi Colton,

Yes for sure. Here we go.

Best Regards

Daniel

Attachments