Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82774members
350584posts

Panel Server and Limit Switch XCKJ10541

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

kaenriquezr
Cadet
Cadet
0 Likes
2
290

Panel Server and Limit Switch XCKJ10541

Dear all,

 

For developing some wireless solutions, we've been wondering if Panel Server can connect to Telemecanique Limit Switches such as XCKJ10541 (or similar).

 

Thanks in advance!

 

BR.

Tags (1)
2 Replies 2
Thierry_Baudard
Lieutenant Lieutenant
Lieutenant
0 Likes
0
271

Re: Panel Server and Limit Switch XCKJ10541

Hello Katherine,

 

wireless Limit Switch XCKJ10541 is not supported by Panel Server,

 

The best way to know if a wireless  is supported by  Panel Server is to refer to the release note which embed the list of supported product

 

PAS600: DOCA0178EN-xx (currently, xx=03 for the last version) 

PAS800: DOCA0248EN-xx (currently, xx=00 for the last version)

 

BR

Thierry BAUDARD
Digital Power Technical Pre sale support International Hub
Tags (1)
Romain_Polette
Sisko Sisko
Sisko
0 Likes
0
269

Re: Panel Server and Limit Switch XCKJ10541

Hello @kaenriquezr , 


The XCKJrange from Industry is not a wireless sensor. We need more precision about the goal of your system.

 

It may be possible to connect the NC/NO output of the sensor to the Digital Inputs of a PAS600L or PAS800L (each gateway has only 2x DI). You must ensure that the sensor can support 24DC voltage.

 

Once you have connected the XCKJ to the DI of the Panel Server you can commission the DI with EcoStruxure Power Commission (DI commissioning with Web Pages will come later).

 

DI status can be viewer on EPC and are also available through Modbus Registers.

 

Regards, 

 

Romain POLETTE - Global Expert Technical Support - Digital Power Division
38EQI - Eybens - France
Tags (1)