Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84796members
354244posts

FDM128 with Panel server 600

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Solved
CharlieKnight
Lieutenant JG
Lieutenant JG
0 Likes
7
1194

FDM128 with Panel server 600

Hello Expert team,

 

Can I connect FDM128 to a Panel server 600 to display the data on the front face of my panel?

 

Best regards

Charlie

Tags (1)

Accepted Solutions
Romain_Polette
Sisko Sisko
Sisko
0 Likes
0
1085

Re: FDM128 with Panel server 600

Hello @CharlieKnight , 

 

It is possible by using the latest firmware version on FDM128 and PAS600 with a limitation of wireless devices displayed (PowerTag, HeatTag,TH110, and CL110).

 

PAS600 last FW.

FDM128 last FW

 

Panel Server Release Notes 

FDM128 Release Notes 

 

Regards,

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France

See Answer In Context

Tags (1)
Romain_Polette
Sisko Sisko
Sisko
0 Likes
5
850

Re: FDM128 with Panel server 600

Hello @CharlieKnight and @Olivier_GARAULT , 

Quick update on the topic.

It seems that FDM128 v8.0.28 is not yet compatible with the PAS600 001.003.001.

We need to wait the next FDM128 release (8.0.29 or later).

Regards, 

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France

See Answer In Context

Tags (1)
7 Replies 7
Romain_Polette
Sisko Sisko
Sisko
0 Likes
0
1086

Re: FDM128 with Panel server 600

Hello @CharlieKnight , 

 

It is possible by using the latest firmware version on FDM128 and PAS600 with a limitation of wireless devices displayed (PowerTag, HeatTag,TH110, and CL110).

 

PAS600 last FW.

FDM128 last FW

 

Panel Server Release Notes 

FDM128 Release Notes 

 

Regards,

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France
Tags (1)
Romain_Polette
Sisko Sisko
Sisko
0 Likes
5
851

Re: FDM128 with Panel server 600

Hello @CharlieKnight and @Olivier_GARAULT , 

Quick update on the topic.

It seems that FDM128 v8.0.28 is not yet compatible with the PAS600 001.003.001.

We need to wait the next FDM128 release (8.0.29 or later).

Regards, 

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France
Tags (1)
Olivier_GARAULT
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
2
846

Re: FDM128 with Panel server 600

Bonjour, 

 

Merci pour le renseignement.

 

Pour information, on vient d'apprendre que le Panel Server n'est pas encore qualifié pour les enveloppes Okken. 
La consigne est de continuer à utiliser le PTL.

 

On fera quand même des tests avec la prochaine version du FDM128.

Tags (1)
sesa157458_brid
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
1
760

Re: FDM128 with Panel server 600

I am really surprised by the previous answer that PAS is not validated inside Okken, can someone provide what is the real status ?

 

Tags (1)
Thierry_Baudard
Lieutenant Lieutenant
Lieutenant

Re: FDM128 with Panel server 600

Hello,

 

There is confusion in the previous message published by Olivier Garault.

Olivier refers to the validation of Panel Server into the SMD solution which is a thermal monitoring solution based on TH110 and whose validation is currently in progress (and not validation in the OKKEN enclosure).

So, obviously, Panel Server fulfills all the conditions, validation and certification to be installed in the OKKEN standard. There is no problem !

 

Thierry BAUDARD
Digital Power Technical Pre sale support International Hub
Tags (1)
sesa242973_brid
Ensign Ensign
Ensign
0 Likes
1
572

Re: FDM128 with Panel server 600

What is the actual status of this point?

I go to a panel builder tomorrow and this is one of the topics we need to solve.

 

BR Geeke

Tags (1)
Romain_Polette
Sisko Sisko
Sisko

Re: FDM128 with Panel server 600

Hi @sesa242973_brid , 

It seems that the latest version of the FDM128 application is now available:

https://www.se.com/fr/fr/download/document/EnerlinX_FDM128_software/

 

I have not yet tested it but normally FDM128 v8.0.30 should work with Panel Server.

Capture d’écran 2022-06-29 160546.jpg

Regards,

 

Romain POLETTE - Solution architect - France Operation
Intencity - Grenoble - France
Tags (1)