Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
It's your place to connect with experts and peers, get continuous support, and share knowledge.
Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.
You can subscribe to this forum after you log in or create your free account..
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.
Already have an account? Login
Hello Expert team,
Can I connect FDM128 to a Panel server 600 to display the data on the front face of my panel?
Best regards
Charlie
Hello @CharlieKnight ,
It is possible by using the latest firmware version on FDM128 and PAS600 with a limitation of wireless devices displayed (PowerTag, HeatTag,TH110, and CL110).
Regards,
Hello @CharlieKnight and @Olivier_GARAULT ,
Quick update on the topic.
It seems that FDM128 v8.0.28 is not yet compatible with the PAS600 001.003.001.
We need to wait the next FDM128 release (8.0.29 or later).
Regards,
Hello @CharlieKnight ,
It is possible by using the latest firmware version on FDM128 and PAS600 with a limitation of wireless devices displayed (PowerTag, HeatTag,TH110, and CL110).
Regards,
Hello @CharlieKnight and @Olivier_GARAULT ,
Quick update on the topic.
It seems that FDM128 v8.0.28 is not yet compatible with the PAS600 001.003.001.
We need to wait the next FDM128 release (8.0.29 or later).
Regards,
Bonjour,
Merci pour le renseignement.
Pour information, on vient d'apprendre que le Panel Server n'est pas encore qualifié pour les enveloppes Okken.
La consigne est de continuer à utiliser le PTL.
On fera quand même des tests avec la prochaine version du FDM128.
I am really surprised by the previous answer that PAS is not validated inside Okken, can someone provide what is the real status ?
Hello,
There is confusion in the previous message published by Olivier Garault.
Olivier refers to the validation of Panel Server into the SMD solution which is a thermal monitoring solution based on TH110 and whose validation is currently in progress (and not validation in the OKKEN enclosure).
So, obviously, Panel Server fulfills all the conditions, validation and certification to be installed in the OKKEN standard. There is no problem !
What is the actual status of this point?
I go to a panel builder tomorrow and this is one of the topics we need to solve.
BR Geeke
Hi @sesa242973_brid ,
It seems that the latest version of the FDM128 application is now available:
https://www.se.com/fr/fr/download/document/EnerlinX_FDM128_software/
I have not yet tested it but normally FDM128 v8.0.30 should work with Panel Server.
Regards,
User | Count |
---|---|
41 | |
29 | |
28 | |
20 | |
18 | |
15 |
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.