Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84710members
354100posts

Com'X510 load shedding possible?

Gateways and Energy Servers

Get expert answers to your questions regarding Schneider Electric Gateways & Energy Servers, from product selection to implementation and troubleshooting. Collaborate with a global community of experts and peers, get support and share your experiences by subscribing to the Schneider Electric Community Gateways and Energy Servers forum today.

Solved
EvonneYin
Ensign Ensign
Ensign
0 Likes
5
310

Com'X510 load shedding possible?

Hi,

Can the Com'X510 do load shedding? Since it is to replace EGX300, how would the Com'X510 perform in load shedding application similar to an EGX300+SIM10M?

Please advise.

Evonne


Accepted Solutions
sesa41698_bridg
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
251

Re: Com'X510 load shedding possible?

Hello Evonne

How do you operate load shedding with an EGX300 ?

How do you write the modbus request ?

FYI : we must have to wait until end of Q12016 in order to get a full EGX300 replacement by the Com'X 510

(especially the HTML custom pages)

     Regards

     Jef

See Answer In Context

5 Replies 5
sesa41698_bridg
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
252

Re: Com'X510 load shedding possible?

Hello Evonne

How do you operate load shedding with an EGX300 ?

How do you write the modbus request ?

FYI : we must have to wait until end of Q12016 in order to get a full EGX300 replacement by the Com'X 510

(especially the HTML custom pages)

     Regards

     Jef

Adrian_Dicea
Janeway Janeway
Janeway
0 Likes
0
251

Re: Com'X510 load shedding possible?

You need internal scripting or scheduler capability on Com'X to trigger Digital Outputs (plus Digital Outputs module).

EGX300 or Com'X 510 by themselves cannot do load shedding. There must be external Client to trigger the Digital Outputs.

sesa57006_bridg
Crewman Crewman
Crewman
0 Likes
2
251

Re: Com'X510 load shedding possible?

Jef,

ABB Emax 2 trip units have load shedding capabilities in the trip unit with ability of utilizing communications (not hardwire) to feeders. Could be very interesting for similar functionality via Com'X communication.  

Ekip Power Controller - Emax 2 (ABB SACE Low Voltage Circuit Breakers)

sesa41698_bridg
Lt. Commander Lt. Commander
Lt. Commander

Re: Com'X510 load shedding possible?

Jonathan FYI :

In the version 2.1.7, We have introduced a Lua engine.

This engine in only used today for generating events that can be send to RSP application.

==> Thus the Lua engine is not directly available for the installer.

(the event are configured using a blockly editor that generate safe Lua script)

In the futures releases, we should improve

  1. The event engine in order to enable to send the event to other destination (SMTP for instance)
  2. The Lua engine to enable some simple control


NOTE : this is just my technical comments, if you want more information please contact mkt (James Jeanette)

LazCM_175878
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
251

Re: Com'X510 load shedding possible?

Hello

This an excellent idea which can be implemented much easier in Smart Panel  architecture.

LCM