Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84384members
353574posts

wireless thermostat

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

Haorld
Cadet
Cadet
0 Likes
7
2314

wireless thermostat

Wireless themostat is becoming popular in markets.

Do SE have this kind of function for thermostat?

Tags (1)
7 Replies 7
CraigEl
Administrator Administrator
Administrator
5
2312

Re: wireless thermostat

SE8000 has Zigbee and WiFi options

Tags (1)
Yi_HU
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: wireless thermostat

TH900 series thermostat can offer Zigbee 3.0 and Modbus communication.

This thermostat can support PTAC, Fan Coil, Heat Pump and Gas/Oil Furnace applications.

 

Tags (1)
GrzegorzLuba
Captain | EcoXpert Master Captain | EcoXpert Master
Captain | EcoXpert Master
0 Likes
3
2075

Re: wireless thermostat

TH900 is a schneider electric product?

Tags (1)
sesa496941_brid
Cadet
Cadet
0 Likes
1
2073

Re: wireless thermostat

Yes, the TH903-ZPM-W is a Zigbee & Modbus Thermostat.

 

You can find attached the datasheet.

 

Attachments
Tags (1)
jgilmartin_west
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master
0 Likes
0
2045

Re: wireless thermostat

The SE8000 series with the wifi adapter work pretty good. Long range too.

 

Tags (1)
Yi_HU
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
0
2010

Re: wireless thermostat

yes, you can find the literature on exchange and SE.com

Tags (1)
DavidChild
Sisko Sisko
Sisko
0 Likes
0
826

Re: wireless thermostat

Hi @Kirk69 ,

 

The Honeywell T9 seems to be home heating solution that works with Alexa, Google Assistant etc.

 

Have you looked at the Wiser solution:

This is the UK version of the product, there may be a version for your region https://wiser.draytoncontrols.co.uk/

Tags (1)