Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84630members
353954posts

Which temperature sensor is for AS-B?

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

Solved
Boris_Horvat
Ensign
Ensign
0 Likes
2
1042

Which temperature sensor is for AS-B?

Hello.

 

I'm looking for a temperature sensor for example STC for connecting to AS-B controller.

In catalog there are:

- STC100 for TAC Vista, TAC Xenta

- STC200 for TAC I/NET

- STC500 for Andover Continuum

- STC600 for Satchwell

- STC600D for Drayton

 

Which one is for SmartX controller? (AS-B, AS-P, MP-C, MP-V, RPC, MP-IO?

 

Thanks.


Accepted Solutions
Mahmoud_Sayed
Sisko Sisko
Sisko

Re: Which temperature sensor is for AS-B?

Hello,

 

You will find the list of compatible sensors/signals at the specification sheet of each SmartX server, controller or IO module.

 

Please refer to the following Screenshot from  AS-B specification sheet, as an example: 

AS-B supported thermistors.PNG

 

Thanks,

Mahmoud

See Answer In Context

2 Replies 2
Mahmoud_Sayed
Sisko Sisko
Sisko

Re: Which temperature sensor is for AS-B?

Hello,

 

You will find the list of compatible sensors/signals at the specification sheet of each SmartX server, controller or IO module.

 

Please refer to the following Screenshot from  AS-B specification sheet, as an example: 

AS-B supported thermistors.PNG

 

Thanks,

Mahmoud

FirdousKhan
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
1022

Re: Which temperature sensor is for AS-B?

 
Mahmoud helped you to solve your problem. Please click on “Accept as Solution” so other members can find the same solution through the search bar.
 
Thank you!

Best,
Firdous - Animation and Moderation Exchange Community Team