Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84244members
353343posts

The thermostat On automatically as soon as the power is On

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

Solved
JayangaDivya
Ensign Ensign
Ensign
0 Likes
1
420

The thermostat On automatically as soon as the power is On

what is Modbus register TC303-3A4DLMS for auto-on at power-on


Accepted Solutions
CraigEl
Administrator Administrator
Administrator
0 Likes
0
408

Re: The thermostat On automatically as soon as the power is On

There is a configuration parameter for this, however it’s not set via mod bus. See https://community.exchange.se.com/t5/Building-Automation-Knowledge/TC3XX-Thermostat-Operation-After-... for further information.

See Answer In Context

Tags (1)
1 Reply 1
CraigEl
Administrator Administrator
Administrator
0 Likes
0
409

Re: The thermostat On automatically as soon as the power is On

There is a configuration parameter for this, however it’s not set via mod bus. See https://community.exchange.se.com/t5/Building-Automation-Knowledge/TC3XX-Thermostat-Operation-After-... for further information.

Tags (1)