Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84741members
354164posts

Integration document for SP90

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

DonaldLEMENAGE
Ensign Ensign
Ensign

Integration document for SP90

This document describes the integration of the SP90 SmartX Actuator with EcoStruxure Building Operation using the BACnet communication protocol. This document also demonstrates how the Automated Engineering Tool (AET) can be used to quickly import and configure multiple actuators and how the SP90 Smart Widget can be used to change or fine tune operation parameters.

Attachments
3 Replies 3
FirdousKhan
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
1547

Re: Integration document for SP90

@DonaldLEMENAGE  thanks for sharing this with the community 😊

Best,
Firdous - Animation and Moderation Exchange Community Team
sesa382463
Crewman Crewman
Crewman
0 Likes
1
1503

Re: Integration document for SP90

document number.  how was the document number for this document arrived at?

Tags (1)
Simon_Firth
Ensign Ensign
Ensign
0 Likes
0
1499

Re: Integration document for SP90

The document number was generated through symphony I understand.

Mr Valve
Tags (1)