Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84539members
353793posts

How replacing an old Erie Classic style actuator?

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

Solved
Janhavi_Jain
Cadet
0 Likes
2
733

How replacing an old Erie Classic style actuator?

Hello,

 

 

Can a new style Erie Poptop Actuator replace and old Erie Classic style actuator?

 

Thanks

 

Tags (1)

Accepted Solutions
CraigEl
Administrator Administrator
Administrator

Re: How replacing an old Erie Classic style actuator?

I don't believe so, you would need to change out the valve as well if you want to use a pop top.

See Answer In Context

2 Replies 2
CraigEl
Administrator Administrator
Administrator

Re: How replacing an old Erie Classic style actuator?

I don't believe so, you would need to change out the valve as well if you want to use a pop top.

MarkSarna
Cadet
Cadet
0 Likes
0
719

Re: How replacing an old Erie Classic style actuator?

The Erie Classic style valve and actuator assemblies were built where the actuator was permanently mounted to the valve.  The newer Erie PopTop style valve and actuators are built so the actuator can be removed and replaced while the valve stays connected to the pipes.  Therefore, PopTop style actuators are not compatible with the Classic style models.

 

For the Erie Classic valves, their are rebuild kits available, see attached.  If the valve is sweat end, replacement with an inverted flare style valve body can be an easier replacement option due to the inverted flare union fittings and longer overall length.  

Valve and Actuator Expert
Attachments
Tags (1)