Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84267members
353374posts

How many SP90’s can I connect under one network ?

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

Solved
Esperanto
Lieutenant JG
Lieutenant JG
0 Likes
2
856

How many SP90’s can I connect under one network ?

Hello,

 

Could you please give me guidance to size SP90 network?

 

Best regards

Espé

Tags (1)

Accepted Solutions
CraigEl
Administrator Administrator
Administrator

Re: How many SP90’s can I connect under one network ?

This probably depends on whether Modbus or BACnet is being used. Since it doesn't state the unit load of the device, it's best to assume a UL of 1 and therefore a maximum of 32 devices.

 

This is also noted on page 7 the Product Manual

 

See Answer In Context

2 Replies 2
CraigEl
Administrator Administrator
Administrator

Re: How many SP90’s can I connect under one network ?

This probably depends on whether Modbus or BACnet is being used. Since it doesn't state the unit load of the device, it's best to assume a UL of 1 and therefore a maximum of 32 devices.

 

This is also noted on page 7 the Product Manual

 

CraigEl
Administrator Administrator
Administrator

Re: How many SP90’s can I connect under one network ?

I've created a Knowledge Base article that provides further guidance on this.