Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84386members
353577posts

EcoStruxure Power Design - Ecodial INT 4.9.7 - The CIRCUIT NAME is now as part of the Data Table and Solution Table

EcoStruxure Power Design Forum

Collaborate with your peers on Electrical Network Design and Calculation Software(Ecodial, Electrical Calculation Tools) - ask questions and get answers from Schneider Electric experts and peers. Share your experience.

Genghiz
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
242

EcoStruxure Power Design - Ecodial INT 4.9.7 - The CIRCUIT NAME is now as part of the Data Table and Solution Table

The CIRCUIT NAME is now as part of the Data Table and Solution Table.

 

  • Draw the electrical network, on the Ecodial application (at the Design & Sizing Tab) as per the requirements.
  • Provide all the necessary inputs to the loads and circuits. 
    • DATA TABLE can also be used to provide inputs for the “components like Cable, load, protection and so on.”

 

  • Calculate the project as usual.
  • Once after the successful completion of the project calculation; As part of the report generation, please click on the SOLUTION TABLE.
  • We can see the component results (solutions) are grouped as per their CIRCUIT NAME.

 

Data Table - Cable component association with Circuit NameData Table - Cable component association with Circuit Name

 

 

Additional Benefit:

 

All the content of the Data Table & Solution Table can be exported in EXCEL, and they can be easily recognized as per the associated “CIRCUIT NAME” and using their “COMPONENT NAME.”

Tags (1)