Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84783members
354229posts

EcoStruxure Power Design - Ecodial INT 4.9.7 - How to change the REPORT language?

EcoStruxure Power Design Forum

Collaborate with your peers on Electrical Network Design and Calculation Software(Ecodial, Electrical Calculation Tools) - ask questions and get answers from Schneider Electric experts and peers. Share your experience.

Genghiz
Lt. Commander Lt. Commander
Lt. Commander

EcoStruxure Power Design - Ecodial INT 4.9.7 - How to change the REPORT language?

The latest version of the Ecodial application is working in 6 languages. They are English, French, Spanish, Turkish, Portugese and Russian.

 

So, we can change and generate the "project report" in different language than the language of the application.

 

Let us see, 

How to select and change the different language for the "Project Report.”

 

Step 1: 

Draw the electrical network as per the requirement and calculate the project.

 

Step 2 : 

After the successful calculation, kindly switch to “Report” tab...Then the application will automatically generate report in default language.

 

Step 3 :

We can see at the Left-hand side, there is an option to change the "Report language."

 

Report - Language Selection.png

 

 

Step 4 :

Change the language (ex. Turkish) and click on the Generate button. The project report will be generated for the selected language.

Attachments
Tags (1)